Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Implemtation of AXI without SDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 396 views
  • Users 0 members are here
Related

Implemtation of AXI without SDK

e14 Contributor
e14 Contributor over 13 years ago

Hey all,

I'm building a software project without Xilinx SDK. I'm using the ARM DS-5 for building the software. Unfortunately I have some problems implementing the PL there.

When I'm using SDK it is not a problem to connect my IP with AXI to the PS.

Unfortunately if I'm using DS-5 I cannot read the values of my IP registers.

Did anyone already implement some IP using AXI with some different compiler than SDK?
I guess I have to write some special registers first, but I don't find any documentation about this problem.

I hope you understand what I'm trying to say ;-)

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 13 years ago

    Hi Schlauby,

    You will need to make sure that your PL is configured with the Bitstream.

    You can do this using USB-JTAG from SDK or using iMPACT tools.

    You can also do this from software through the PCAP interface.  An example of this is given within the Fisrt Stage Boot Loader code template.  Here you will find a image_mover.c file which has a PartitionMove() function defined as this:

    u32 PartitionMove(u32 ImageAddress, int PartitionNum)

    This function is responsible for handling the partition data read from boot media and when it locates a bitstream file, it transfers the bitstream data to the PCAP interface in order to configure the PL.  If you are not programming your PL already, you could take a look at this FSBL code to see if you can adapt some of this into your application.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 13 years ago

    Hi Schlauby,

    You will need to make sure that your PL is configured with the Bitstream.

    You can do this using USB-JTAG from SDK or using iMPACT tools.

    You can also do this from software through the PCAP interface.  An example of this is given within the Fisrt Stage Boot Loader code template.  Here you will find a image_mover.c file which has a PartitionMove() function defined as this:

    u32 PartitionMove(u32 ImageAddress, int PartitionNum)

    This function is responsible for handling the partition data read from boot media and when it locates a bitstream file, it transfers the bitstream data to the PCAP interface in order to configure the PL.  If you are not programming your PL already, you could take a look at this FSBL code to see if you can adapt some of this into your application.

    Regards,

    -Kevin