Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Run QT Software on Linaro
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1204 views
  • Users 0 members are here
Related

Run QT Software on Linaro

e14 Contributor
e14 Contributor over 14 years ago

I want to design a software with GUI and let it execute on my zed. So I have gotten a Linaro running on zed and a application designed with QT.

Now my question is how to compile and execute this app. Should I use the arm-xilinx cross-compiler? Any libs or sources of QT should I add in the Linaro rootfs? Can a QT Creator run on a zedboard with Linaro just like it runs on the PC with Ubuntu?

Does anybody konw the answers?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    It appears that you can just point QT Creator to a different compiler.  Ref link:

    http://doc.qt.digia.com/4.7-snapshot/qt-embedded-crosscompiling.html

    You can set QT to compile all of the libraries into your binary if you want, or you can copy all of the libraries you are using to your roomfs (I would recommend the former).

    I would not recommend running QT Creator on the zedboard itself, as you are not going to get any where near the performance of your PC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for your advices, Tim.
    If I want to compile the QT app, which cross-compiler should I use, The arm-xilinx-linux-gnueabi or Linaro toolchain? I was trying to compile an app using Xilinx toolchain and it failed to run on Linaro. So I guess the latter can be used to do the job. And is that possible to install the Qt-lib on Linaro derectly so that I can both complie and run Qt apps on my zed?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    You certainly could get the qt compiler and associated libraries moved over to your Zedboard if you wanted to - I personally prefer to cross-compile as it usually is much faster (but if you are talking about small applications then it really shouldn't make much of a difference).

    As for which cross compiler to use, I have had the most luck with the arm-xilinx-linux-gnueabi toolchain - but I haven't compiled a qt program yet.

    Give them both a shot and let us know which one works!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi , I am also trying to do the same stuffs on My xilinx zc702 board.

    But I got stuked and it was not getting fired up.

    Below are the steps I have tried to build and compile the same.

    1) qt-everywhere-opensource-src-4.7.3.tar.gz(Extract It on host)
    2) qmake.conf:
            Replace: arm-none-linux-gnueabi-gcc by arm-linux-gnueabihf-gcc

    3) Set the path:
        export CROSS_COMPILE=arm-linux-gnueabihf-
        export PATH=/usr/bin:$PATH
        export ZYNQ_QT_BUILD=/home/user/qt-everywhere-opensource-src-4.7.3
        export ZYNQ_QT_INSTALL=/usr/local/Trolltech
        export PATH=$ZYNQ_QT_INSTALL/bin:$PATH

    4) ./configure -embedded armv7l -xplatform qws/linux-arm-gnueabi-g++ -little-endian -opensource -host-little-endian -confirm-license -prefix $ZYNQ_QT_INSTALL -qt-zlib -qt-libtiff -qt-libpng -qt-libmng -qt-libjpeg -no-openssl -no-nis -no-cups -iconv -no-pch -no-dbus -qt-freetype -no-opengl -qt-gfx-linuxfb -qt-gfx-vnc -qt-gfx-qvfb
    (This we tried with arm as well)

    5)  make
        make -install
        copied all the libraries(from /usr/local/Trolltech) to the target board at (/usr/local/Trolltech).

    6) ./appname -qws -display QVFb:0
         error:  driver cannot connect
         Aborted
    (Cause:This I think we donu2019t have to use as we are running linux so have to use LinuxFb)

        ./appname  -qws LinuxFb:mmwidth=1024:mmheight=768
        this does not give any error but, it's not launching the GUI but printing the log messages in terminal.

    can you tell What we are missing here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Check out buildroot:
    http://buildroot.uclibc.org/u200E
    It creates a root filesystem, cross compiling all the libraries you select in a menu-driven (not unlike the Linux kernel configuration) build system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi ,
    As we are using the Linaro Ubuntu Desktop so they are providing the pre built Linaro file system alongwith the Xilinx board but ucilibc is different file system so whether it will work fine on Zed Board with GUI desktop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hello! I want to run Qt applications on my zedboard. But I don't know how to install the Qt tool chains. I have downloaded "qt-embedded-linux-opensource-4.5.3.tar.gz", and installed arm-linux-gnueabi-gcc and arm-linux-gnueabi-g++. Then I used command "./configure -embeded arm" to configure. At this time, errors occurred, such as: arm-linux-g++ can not found. So, I want to know how to install Qt cross compiling environment. I just want to create and compile my app on PC host, then copy the result to zedboard with linux OS. Can anyone help me ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi, i have the same issue, is there any sollution yet ?