Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Run QT Software on Linaro
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1205 views
  • Users 0 members are here
Related

Run QT Software on Linaro

e14 Contributor
e14 Contributor over 14 years ago

I want to design a software with GUI and let it execute on my zed. So I have gotten a Linaro running on zed and a application designed with QT.

Now my question is how to compile and execute this app. Should I use the arm-xilinx cross-compiler? Any libs or sources of QT should I add in the Linaro rootfs? Can a QT Creator run on a zedboard with Linaro just like it runs on the PC with Ubuntu?

Does anybody konw the answers?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    It appears that you can just point QT Creator to a different compiler.  Ref link:

    http://doc.qt.digia.com/4.7-snapshot/qt-embedded-crosscompiling.html

    You can set QT to compile all of the libraries into your binary if you want, or you can copy all of the libraries you are using to your roomfs (I would recommend the former).

    I would not recommend running QT Creator on the zedboard itself, as you are not going to get any where near the performance of your PC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for your advices, Tim.
    If I want to compile the QT app, which cross-compiler should I use, The arm-xilinx-linux-gnueabi or Linaro toolchain? I was trying to compile an app using Xilinx toolchain and it failed to run on Linaro. So I guess the latter can be used to do the job. And is that possible to install the Qt-lib on Linaro derectly so that I can both complie and run Qt apps on my zed?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for your advices, Tim.
    If I want to compile the QT app, which cross-compiler should I use, The arm-xilinx-linux-gnueabi or Linaro toolchain? I was trying to compile an app using Xilinx toolchain and it failed to run on Linaro. So I guess the latter can be used to do the job. And is that possible to install the Qt-lib on Linaro derectly so that I can both complie and run Qt apps on my zed?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    You certainly could get the qt compiler and associated libraries moved over to your Zedboard if you wanted to - I personally prefer to cross-compile as it usually is much faster (but if you are talking about small applications then it really shouldn't make much of a difference).

    As for which cross compiler to use, I have had the most luck with the arm-xilinx-linux-gnueabi toolchain - but I haven't compiled a qt program yet.

    Give them both a shot and let us know which one works!