Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zedboard QSPI FSBL with Bare Metal Application and bitstream
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 1608 views
  • Users 0 members are here
Related

Zedboard QSPI FSBL with Bare Metal Application and bitstream

e14 Contributor
e14 Contributor over 14 years ago

Hi All.

I am wondering if anyone has a bare-metal application plus bitstream booting successfully from QSPI (using ISE14.1)?

I have an application that consists of both bare-metal implementation and Programmable Logic.  To date, I have been using the SDK tools to download the bistream, and then using SDK->Project Explorer->Right Click on Program->Run As->Launch on Hardware.

I would now like to have the .bit and .elf included in the QSPI so that the board can boot from it.

Here's what I've done to date:
1a.  Added and successfully built a Zynq FSBL project.
1b.  I have not made ANY code changes to FSBL source code...  but I wonder if that is necessary to somehow tell the FSBL which bitstream and elf to use.

2a. SDK->Xilinx Tools->Create Boot image.
2b.  In the above menu, I select the FSBL elf file as the fsbl.elf of step#1.
2c.  In the above menu, I add (2) partitions.  First, the bitstream from the design.  Second, the bare-metal application .elf.
2d.  I then select an output file location.
2e.  The output of step #2 creates a .mcs file.

3a.  SDK->Xilinx Tools->Program Flash
3b.  I select the .mcs file created in step #2 and select 'Enter'.
3c.  This starts the process (shown in the console) but it ends up crashing after about 30 seconds with the following Windows Error message.  "zynq_flash.exe has encountered a problem and needs to close"

Looking at the console, no errors are shown, and the console says it erases the QSPI 100%, but there are not any  messages about programming the QSPI.

Any suggestions are much appreciated, thanks!


-------Console output below---------
JTAG chain configuration
--------------------------------------------------
Device   ID Code        IR Length    Part Name
1       4ba00477           4        Cortex-A9
2       03727093           6        XC7Z020

CortexA9 Processor Configuration
-------------------------------------
Version.............................0x00000003
User ID.............................0x00000000
No of PC Breakpoints................6
No of Addr/Data Watchpoints.........1
BOOT_MODE REG = 0x00000000
Info:Firmware image : C:Xilinx14.114.1ISE_DSISEdatacsecseflashzynq7000qspi_single.bin.
Downloading Program -- C:Xilinx14.114.1ISE_DSISEdatacsecseflashzynq7000qspi_single.bin
tsection, .text: 0xfffc4800-0xfffd230f
tsection, .rodata: 0xfffd2310-0xfffd4628
tsection, .data: 0xfffd462c-0xfffd4e6f
tsection, .u_boot_cmd: 0xfffd4e70-0xfffd503b
tsection, .bss: 0xfffd5040-0xfffd729f
Setting PC with Program Start Address 0xfffc4800
Info:Performing Erase operation.

100% Info:Erase operation completed successfully.
100%

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    This link should work: http://www.zedboard.org/design/1521/11

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    This link should work: http://www.zedboard.org/design/1521/11

     

    -Gary