Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AXI in ZYNQ
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 363 subscribers
  • Views 2909 views
  • Users 0 members are here
Related

AXI in ZYNQ

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I am doing interface between ps to pl in ZYNQ processor. I need some clarifications on interface.
1. what is the frequency of AXI4 clock frequency.
2. for interface have 3 ways like (GPIO, ACP), I need some technical document to use the methods in vivado 2014.1.

Thanks & Regards
Ashwak ali S.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The frequency of the AXI clock in your design depends on your hardware implementation. The Zynq is a programmable device and you can set the AXI clock frequency based on your design as well as the maximums for your specific device and speed grade.

     

    For the Zynq device on the ZedBoard and MicroZed the default clock rate defined using the Vivado tools will be 100 MHz.

     

    You might want to take the time to run through some of the training material available. A good place to start would be the Avnet Zynq Speedway workshops:

     

    Developing ZynqRegistered-7000 All Programmable SoC Software (Vivado 2013.3)

     

    Developing ZynqRegistered-7000 All Programmable SoC Hardware (Vivado 2013.3)

     

    which will give you a better idea of how the various interfaces work. Once you have generated a working Zynq hardware design in Vivado and 'exported' this design to the SDK you can open up the system.mss file. Here you will find links to example code for each of the available peripherals.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The frequency of the AXI clock in your design depends on your hardware implementation. The Zynq is a programmable device and you can set the AXI clock frequency based on your design as well as the maximums for your specific device and speed grade.

     

    For the Zynq device on the ZedBoard and MicroZed the default clock rate defined using the Vivado tools will be 100 MHz.

     

    You might want to take the time to run through some of the training material available. A good place to start would be the Avnet Zynq Speedway workshops:

     

    Developing ZynqRegistered-7000 All Programmable SoC Software (Vivado 2013.3)

     

    Developing ZynqRegistered-7000 All Programmable SoC Hardware (Vivado 2013.3)

     

    which will give you a better idea of how the various interfaces work. Once you have generated a working Zynq hardware design in Vivado and 'exported' this design to the SDK you can open up the system.mss file. Here you will find links to example code for each of the available peripherals.

     

    -Gary