Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problems with release 14.3
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 971 views
  • Users 0 members are here
Related

problems with release 14.3

e14 Contributor
e14 Contributor over 14 years ago

hello,

I loaded R 14.3 both on Windows 7 and on Linux-Ubuntu 12.04

then to test it I followed the zynq geek hello world

I got no errors with the Windows version, but with Linux (on two different computers) when I launch the bit stream generator I always got this error:

[Edk 24-166] (generate target): failed to execute XPS script. Please check for any errors reported by XPS application in the console:
[/home/zedboard/working_area/xilinx_prj/zed_first_again/zed_srcs/sources_1/edk/proc_module/__xps/pa/_proc_module_synth.tcl]

in linux I launch planAhed as root

I have this error with linux under webPACK license, but I have no errors with windows 7 both with node locked and with web pack license

do I have to do some workaround?


       Roberto

Post Scriptum:
there is some mess with latin and chinese character in the blog

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Roberto,

    I'll write up a "Bringing up 2012.3 on Ubuntu" How-to and see if I run into these same errors.  I had not seen anything like this with 2012.2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi zynqgeek,
    _
    yes, I confirm I didn't had this problem with 14.2 and I do not have any error with 14.3 in Windows (webpack and node locked license)
    _
    I just have this problem with two different ubuntu 12.04 systems (webpack license)
    _
    I just tried your hello world example to test the 14.3 and I had that problem
    _
      Best regards,
    ____Roberto

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 14 years ago

    Hi Roberto,

    I noticed after clicking on your post, that I too am now looking at pages with mixed Chinese characters.  Look for the English hyperlink on the top level forums page. 

    After clicking the "English" link, the forum contents should revert back to Latin characters for you.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi,

    I had the same error in a Windows 7 machine.  For me it was caused by the file path being too long (because the tools decide to bury every file in a million sub-directories).  If this isn't the cause try looking at the "Tcl Console" at the bottom of the screen to see if there are any warnings/errors reported.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi m.russell,
    .
    I had no problems with Windows 7 64, I just have problems with Linux (Ubuntu) version
    .
    I swapped back to release 14.2; apart that there is no direct management for the ZedBoard I think that is a better release
    .
    BR,
    .   Roberto

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Had the same problem, the solution that worked for me: cd /usr/bin
    sudo ln -s make gmake

    I'm working on ubuntu 12.04lts
    source: http://forums.xilinx.com/t5/Design-Planning/XPS-application-ahead/m-p/264108/highlight/true#M1497