Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problems with release 14.3
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 971 views
  • Users 0 members are here
Related

problems with release 14.3

e14 Contributor
e14 Contributor over 14 years ago

hello,

I loaded R 14.3 both on Windows 7 and on Linux-Ubuntu 12.04

then to test it I followed the zynq geek hello world

I got no errors with the Windows version, but with Linux (on two different computers) when I launch the bit stream generator I always got this error:

[Edk 24-166] (generate target): failed to execute XPS script. Please check for any errors reported by XPS application in the console:
[/home/zedboard/working_area/xilinx_prj/zed_first_again/zed_srcs/sources_1/edk/proc_module/__xps/pa/_proc_module_synth.tcl]

in linux I launch planAhed as root

I have this error with linux under webPACK license, but I have no errors with windows 7 both with node locked and with web pack license

do I have to do some workaround?


       Roberto

Post Scriptum:
there is some mess with latin and chinese character in the blog

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Had the same problem, the solution that worked for me: cd /usr/bin
    sudo ln -s make gmake

    I'm working on ubuntu 12.04lts
    source: http://forums.xilinx.com/t5/Design-Planning/XPS-application-ahead/m-p/264108/highlight/true#M1497

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Had the same problem, the solution that worked for me: cd /usr/bin
    sudo ln -s make gmake

    I'm working on ubuntu 12.04lts
    source: http://forums.xilinx.com/t5/Design-Planning/XPS-application-ahead/m-p/264108/highlight/true#M1497