Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zynq 7000 Flashing Using Xilinx SDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 552 views
  • Users 0 members are here
Related

Zynq 7000 Flashing Using Xilinx SDK

e14 Contributor
e14 Contributor over 12 years ago

Hello All,

I am trying to program flash memory with the following:
1) System.bit file that has the hardware
2) bootloop.elf - FSBL (frist stage boot loop) created in SDK nothing was changed
3) helloword.elf created in the SDK

I am trying to figure out where to find the offset in the bootloop (FSBL) for the application. What address does the boot loop start reading from I don't know where that is in the code.

Please help.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You can use the "Create Boot Image" utility in the SDK under 'Xilinx Tools' to create the boot image and the "Program Flash" utility, again in the SDK under 'Xilinx Tools' to write the image to the QSPI Flash..

     

    You don't mention which Zynq board you are using but Tutorial 04 for the MicroZed board found here details how to step through the process:

     

    http://www.zedboard.org/design/1519/10

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You can use the "Create Boot Image" utility in the SDK under 'Xilinx Tools' to create the boot image and the "Program Flash" utility, again in the SDK under 'Xilinx Tools' to write the image to the QSPI Flash..

     

    You don't mention which Zynq board you are using but Tutorial 04 for the MicroZed board found here details how to step through the process:

     

    http://www.zedboard.org/design/1519/10

     

    -Gary