Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zynq FSBL cannot read BOOT.bin from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 364 subscribers
  • Views 3879 views
  • Users 0 members are here
Related

Zynq FSBL cannot read BOOT.bin from SD card

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I also posted my problem in the Xilinx forums (http://forums.xilinx.com/t5/Embedded-Linux/Zynq-FSBL-cannot-read-BOOT-bin-from-SD-card/m-p/522631/highlight/false), but as they couldn't help me yet and it also might be a MicroZed related problem, I'm posting it here now as well.

I have a MicroZed board with a Zynq 7020. I created a Project in Vivado and applied the board definition files provided here: http://zedboard.org/support/documentation/1519. Then I created a FSBL project in the SDK based on that hardware project. As a minimal example I generated a bootimage using the FSBL I generated and the u-boot.elf from the SD card image provided by Avnet, from the same link as above. I enabled the debug output of the FSBL and it tells me this:

Xilinx First Stage Boot Loader
Release 2014.2 Sep 22 2014-14:34:28
Devcfg driver initialized
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD: Unable to open file BOOT.BIN: 3
SD_INIT_FAIL
FSBL Status = 0xA009

This Boot Mode Doesn't Support Fallback
In FsblHookFallback function

I am able to boot from the original BOOT.bin provided by Avnet, so neither my SD card, nor my MicroZed should be broken. As suggested in related threads, I also verified that the CD and WP pins are configured right and that the SD card clock is set to 50MHz. I tried routing the WP pin to an EMIO without any success. I also tried it with and without a .bit file. Is there anything else I could try?

Thanks,
Alain

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    hi Alain, I'm having the exact same problem; how did you use ISE 14.7 to generate the bootimage? can you send detailed instructions? thanks
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    hi Alain,
    I'm having the exact same problem;
    how did you use ISE 14.7 to generate the bootimage?
    can you send detailed instructions? thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    hi Alain,
    I'm having the exact same problem;
    how did you use ISE 14.7 to generate the bootimage?
    can you send detailed instructions? thanks