Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zynq FSBL cannot read BOOT.bin from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 364 subscribers
  • Views 3878 views
  • Users 0 members are here
Related

Zynq FSBL cannot read BOOT.bin from SD card

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I also posted my problem in the Xilinx forums (http://forums.xilinx.com/t5/Embedded-Linux/Zynq-FSBL-cannot-read-BOOT-bin-from-SD-card/m-p/522631/highlight/false), but as they couldn't help me yet and it also might be a MicroZed related problem, I'm posting it here now as well.

I have a MicroZed board with a Zynq 7020. I created a Project in Vivado and applied the board definition files provided here: http://zedboard.org/support/documentation/1519. Then I created a FSBL project in the SDK based on that hardware project. As a minimal example I generated a bootimage using the FSBL I generated and the u-boot.elf from the SD card image provided by Avnet, from the same link as above. I enabled the debug output of the FSBL and it tells me this:

Xilinx First Stage Boot Loader
Release 2014.2 Sep 22 2014-14:34:28
Devcfg driver initialized
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD: Unable to open file BOOT.BIN: 3
SD_INIT_FAIL
FSBL Status = 0xA009

This Boot Mode Doesn't Support Fallback
In FsblHookFallback function

I am able to boot from the original BOOT.bin provided by Avnet, so neither my SD card, nor my MicroZed should be broken. As suggested in related threads, I also verified that the CD and WP pins are configured right and that the SD card clock is set to 50MHz. I tried routing the WP pin to an EMIO without any success. I also tried it with and without a .bit file. Is there anything else I could try?

Thanks,
Alain

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    hi Alain, I'm having the exact same problem; how did you use ISE 14.7 to generate the bootimage? can you send detailed instructions? thanks
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Alain,

      I'm just speculating, but I think the error message might be misleading.  The fact that you are able to run the FSBL indicates that the BOOTROM code was able to load and validate the Boot Header, and was able to load the FSBL to OCM and execute it.  However, when the FSBL attempts to load the next partition, it fails.   That indicates to me that the image is somehow corrupt, so I'm wondering exactly how you generated it?

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    You are right. It was a problem with Vivado. I now use ISE 14.7 to generate the bootimage and that works. Somehow Vivado seems to be broken.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    hi Alain,
    I'm having the exact same problem;
    how did you use ISE 14.7 to generate the bootimage?
    can you send detailed instructions? thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ashahsana
    0 ashahsana over 11 years ago

    Hello
    I am using ISE 14.7. when I am trying to make bootimage it crash.
    I am adding following files
    fsbl.elf
    system.bit
    my_software.elf
    can anyone guide me, what is the problem here
    regards 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adielement
    0 adielement over 1 year ago

    I have same issue. Zynq FSBL cannot load SD Card BOOT.bin. I am getting following error

    Xilinx First Stage Boot Loader
    Release 2019.1 May 15 2025-15:52:49
    Devcfg driver initialized
    Silicon Version 3.1
    Booting Device is MMC
    SD: rc= 0
    MMC Init Done
    Flash Base Address: 0xE0100000
    Reboot status register: 0x60400000
    Multiboot Register: 0x0000C000
    Image Start Address: 0x00000000
    Partition Header Offset:0x00000C80
    Partition Count: 3
    Partition Number: 0
    Header Dump
    Image Word Len: 0x00007002
    Data Word Len: 0x00007002
    Partition Word Len:0x00007002
    Load Addr: 0x00000000
    Exec Addr: 0x00000000
    Partition Start: 0x000005C0
    Partition Attr: 0x00000010
    Partition Checksum Offset: 0x00000000
    Section Count: 0x00000001
    Checksum: 0xFFFEA7E8
    Application
    Handoff Address: 0x00000000
    In FsblHookBeforeHandoff function
    No Execution Address JTAG handoff

    How can I fix this issue. I need to further move towards booting EMMC BOOT.bin in place of SD card BOOT.bin, after resolving this issue.
    Any help in this regard is highly appreciated. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iksevas
    0 iksevas over 1 year ago in reply to adielement

    What type of SD card are you using? Must be SDHC type. I like using SDHC from Sandisk Class 10.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adielement
    0 adielement over 1 year ago in reply to iksevas

    panasonic. it's sdhc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iksevas
    0 iksevas over 1 year ago in reply to adielement

    Have you tried something simple like Hello World and create BOOTIMAGE for that. It should be super simple to do.

    another option is to look at MicroZed Chronicles articles as they will walk you through creating a successful bootable design. 

    Also, have you followed the getting started guide to prove to yourself that this works? This would be with a known good design.