Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Which GPIO connect to LD9
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 696 views
  • Users 0 members are here
Related

Which GPIO connect to LD9

cascade99
cascade99 over 10 years ago

Hi,
On zedboard, it seems LD9 can be turned on/off through PS directly, which is PS-MIO[7], anybody knows which GPIO pin it refers to?
I'm using petalinux 14.4, can I export it from console directly?
Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Lynn,

     

    The gpio offset for PetaLinux 2014.4 seems to be 138. As you have noted LD9 is connected to MIO7. Therefore the GPIO address, using the SysFs subsystem would be 145.

     

    Take a look at the section of the PicoZed FMC Carrier Getting Started Guide, v2.1, starting on page 23, that details interacting with GPIO. It is based on PetaLinux 2014.4 as well. Even though it is targeting the PicoZed FMC Carrier card, and the LED is MIO47 on that board, the method illustrated should work the same on the ZedBoard using 138 + 7 = 145, rather than the 185 address used there:

    http://zedboard.org/sites/default/files/documentations/PicoZed_FMC_CC_GettingStarted_v2_1.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • cascade99
    0 cascade99 over 10 years ago in reply to e14 Contributor

    Thank you very much, Gary. It works great.