Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development GPIO MIOs from linux kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 365 subscribers
  • Views 1110 views
  • Users 0 members are here
Related

GPIO MIOs from linux kernel

oscargomezf
oscargomezf over 10 years ago

Hi,

 

I would like to know how to access to GPIOs MIO from Linux kernel.

 

I'm not completely sure how to do that.

 

I can see in my picoZed in the /sys/class/gpio the folder gpiochip0 and inside this folder the file ngpio with a value of 64. But I not completely sure if this is the MIO GPIOs, because the MIO are 54 GPIOS:

MIO0 pins 0 to 15 -> connected to a 3.3Volts bank
MIO1 pins 16 to 53 -> connected to 1.8 Volts bank
 
Am I right or wrong?
 
Best regards.
  • Sign in to reply
  • Cancel
Parents
  • oscargomezf
    0 oscargomezf over 10 years ago

    Hi,

     

    I was reading the /proc/device-tree/amba/gpio@e000a000 with a width of 64 bits. And I've tried to configure de PS_MIO51 as an input to check the PS_PB button in the PicoZed FMC Carrier V2:

    $ echo 51 > export
    $ echo in > 51/direction
    $ cat 51/value
     
    And when I pressed that button I've got and 1 and when the button is released I've got a 0, So it's working fine. But If I only have 54 GPIOS (From 0 to 53) Whats happen with the GPIOS from 54 to 63? I think It has to be a width of width instead of 54 because it has to be a power of 2 and If you try to access to the pins from 54 to 63 nothing happens, but I'm not completely sure.
     
    Best regards.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • oscargomezf
    0 oscargomezf over 10 years ago

    Hi,

     

    I was reading the /proc/device-tree/amba/gpio@e000a000 with a width of 64 bits. And I've tried to configure de PS_MIO51 as an input to check the PS_PB button in the PicoZed FMC Carrier V2:

    $ echo 51 > export
    $ echo in > 51/direction
    $ cat 51/value
     
    And when I pressed that button I've got and 1 and when the button is released I've got a 0, So it's working fine. But If I only have 54 GPIOS (From 0 to 53) Whats happen with the GPIOS from 54 to 63? I think It has to be a width of width instead of 54 because it has to be a power of 2 and If you try to access to the pins from 54 to 63 nothing happens, but I'm not completely sure.
     
    Best regards.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • oscargomezf
    0 oscargomezf over 10 years ago in reply to oscargomezf

    Sorry, I made a typographic error, and I don't know how to modify this post:

    $ cd /sys/class/gpio
    $ echo 51 > export
    $ echo in > gpio51/direction
    $ cat gpio51/value