Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development microzed running pulsar linux stalls on boot up, UTMP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 760 views
  • Users 0 members are here
Related

microzed running pulsar linux stalls on boot up, UTMP

e14 Contributor
e14 Contributor over 10 years ago

We are running pulsar linux on our microzed processor and having very long boot up times.  The boot process stalls on 

"started Update UTMP about System Runlevel Changes"

Has anyone else run into this?  Does anyone know a solution to this?

 

Here is what we see on boot up:

          Starting Network Service...

         Starting Login Service...
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started Change the tty3 to be the active vt.
[  OK  ] Started Ethernet Bridge Filtering Tables.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started Login Service.
[     *] (2 of 2) A start job is running for Network Service (34s / 1min 53s)gre▒ GRE over IPv4 demultiplexor driver
[  OK  ] Started Open vSwitch Internal Unit.
[  OK  ] Started Network Service.
device eth0 entered promiscuous mode
IPv6: ADDRCONF(NETDEV_UP): br0: link is not ready
         Starting Network Name Resolution...
br0: port 1(eth0) entered forwarding state
br0: port 1(eth0) entered forwarding state
[  OK  ] Reached target Network.r0: link becomes ready
         Starting Open vSwitch...
         Starting Xinetd A Powerful Replacement For Inetd...
         Starting Setup dnsmasq...
[  OK  ] Started Setup dnsmasq.
         Starting LXC Container Initialization and Autoboot Code...
         Starting /etc/rc.local Compatibility...
[  OK  ] Started Network Name Resolution.
[  OK  ] Started Open vSwitch.
[  OK  ] Started Xinetd A Powerful Replacement For Inetd.
[  OK  ] Started /etc/rc.local Compatibility.
         Starting Getty on tty1...
[  OK  ] Started Getty on tty1.
[  OK  ] Reached target Login Prompts.
[  OK  ] Started LXC Container Initialization and Autoboot Code.
[  OK  ] Reached target Multi-User System.
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.
 
Pulsar Linux 7.0.0.11 cube-21-03-16-cube-server ttyPS0
 
 
 
  • Sign in to reply
  • Cancel
  • narrucmot
    0 narrucmot over 10 years ago

    Hello,

    I have noticed this stall during boot at this step and always been told that it is normal.  I will try to find out why from the folks at Wind River.  Do you have a boot time requirement that is not being met, or is this more of a general question?

    Regards,

    Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to narrucmot

    Tom,

    thanks for the response. We don't have a spec but we are building a piece of equipment based on the microzed board and users are going to expect to turn on the instrument and have it running within 15 secs or so.  If the user has to wait much longer than that then they will probably cycle the power to see whats going on.  BTW, the boot time varys greatly.  Some times it takes seconds and sometimes more than a minute.

    Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 10 years ago

    Hi Matt,

    Just because the Pulsar-7 boot stalls at "Started Update UTMP about System Runlevel Changes" doesn't necessarily indicate that is the issue.  That is just the last line of status message that is printed before the kernel continues with other boot tasks.  I spoke to an engineer at Wind River and their suggestion is to install and run the systemd-analyze application to get an idea of where the system is spending its time during boot.  Here are some instructions for downloading, installing, and running the application to generate graphs that can be used analyze the time spent at each boot step:

    # Log in as root and run the following commands
    cube-console dom0
    cube-console essential
    smart update > /dev/null
    smart download systemd-analyze
    mv systemd*.rpm  /var/lib/lxc/cube-server/rootfs/root
    rpm -ihv /var/lib/lxc/cube-server/rootfs/root/systemd-analyze*.rpm
    lxc-attach -n dom0 -- rpm -ihv /var/lib/lxc/cube-server/rootfs/root/systemd-analyze*.rpm
    lxc-attach -n cube-server -- rpm -ihv /root/systemd-analyze*.rpm
    
    
    systemd-analyze plot > /var/lib/lxc/cube-server/rootfs/root/1.svg
    lxc-attach -n dom0 -- systemd-analyze plot > /var/lib/lxc/cube-server/rootfs/root/2.svg
    lxc-attach -n cube-server -- systemd-analyze plot > /var/lib/lxc/cube-server/rootfs/root/3.svg
    cat<<EOF>/var/lib/lxc/cube-server/rootfs/root/0.html
    <img src=1.svg>
    <br>
    <img src=2.svg>
    <br>
    <img src=3.svg>
    EOF
    exit
    exit
    
    
    # Now copy off the data how every you choose.
    scp *.html *.svg YOUR_SERVER:/YOUR_DIR
    
    # Now that you have the files on a different machine use Chrome on the 0.html file
    
    google-chrome 0.html
    
    # You will see a full graph of where all the time was spent in the boot process
    
    
    
    

    For example, here are a couple of example graphs created for Pulsar-7 and Pulsar-8 running on a MicroZed-7010.

    Pulsar-7: http://htmlpreview.github.io/?https://github.com/jwessel/scratch/blob/master/MZ/pulsar-7-7010-boot/0.html

    Pulsar-8: http://htmlpreview.github.io/?https://github.com/jwessel/scratch/blob/master/MZ/pulsar-8-7010-boot/0.html

    It is recommended, if you can, to use Pulsar-8 instead.  Wind River has made some significant improvements to system start in Pulsar-8, and it also prints out much more information about what is going on.

    I hope this helps.

    --Tom