Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development microzed running pulsar linux stalls on boot up, UTMP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 761 views
  • Users 0 members are here
Related

microzed running pulsar linux stalls on boot up, UTMP

e14 Contributor
e14 Contributor over 10 years ago

We are running pulsar linux on our microzed processor and having very long boot up times.  The boot process stalls on 

"started Update UTMP about System Runlevel Changes"

Has anyone else run into this?  Does anyone know a solution to this?

 

Here is what we see on boot up:

          Starting Network Service...

         Starting Login Service...
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started Change the tty3 to be the active vt.
[  OK  ] Started Ethernet Bridge Filtering Tables.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started Login Service.
[     *] (2 of 2) A start job is running for Network Service (34s / 1min 53s)gre▒ GRE over IPv4 demultiplexor driver
[  OK  ] Started Open vSwitch Internal Unit.
[  OK  ] Started Network Service.
device eth0 entered promiscuous mode
IPv6: ADDRCONF(NETDEV_UP): br0: link is not ready
         Starting Network Name Resolution...
br0: port 1(eth0) entered forwarding state
br0: port 1(eth0) entered forwarding state
[  OK  ] Reached target Network.r0: link becomes ready
         Starting Open vSwitch...
         Starting Xinetd A Powerful Replacement For Inetd...
         Starting Setup dnsmasq...
[  OK  ] Started Setup dnsmasq.
         Starting LXC Container Initialization and Autoboot Code...
         Starting /etc/rc.local Compatibility...
[  OK  ] Started Network Name Resolution.
[  OK  ] Started Open vSwitch.
[  OK  ] Started Xinetd A Powerful Replacement For Inetd.
[  OK  ] Started /etc/rc.local Compatibility.
         Starting Getty on tty1...
[  OK  ] Started Getty on tty1.
[  OK  ] Reached target Login Prompts.
[  OK  ] Started LXC Container Initialization and Autoboot Code.
[  OK  ] Reached target Multi-User System.
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.
 
Pulsar Linux 7.0.0.11 cube-21-03-16-cube-server ttyPS0
 
 
 
  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 10 years ago

    Hello,

    I have noticed this stall during boot at this step and always been told that it is normal.  I will try to find out why from the folks at Wind River.  Do you have a boot time requirement that is not being met, or is this more of a general question?

    Regards,

    Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 10 years ago

    Hello,

    I have noticed this stall during boot at this step and always been told that it is normal.  I will try to find out why from the folks at Wind River.  Do you have a boot time requirement that is not being met, or is this more of a general question?

    Regards,

    Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to narrucmot

    Tom,

    thanks for the response. We don't have a spec but we are building a piece of equipment based on the microzed board and users are going to expect to turn on the instrument and have it running within 15 secs or so.  If the user has to wait much longer than that then they will probably cycle the power to see whats going on.  BTW, the boot time varys greatly.  Some times it takes seconds and sometimes more than a minute.

    Matt