Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Picozed CC Gen2 SPI test - via PS (JPS1) and EMIO (JB1) - slow speeds
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 365 subscribers
  • Views 1439 views
  • Users 0 members are here
Related

Picozed CC Gen2 SPI test - via PS (JPS1) and EMIO (JB1) - slow speeds

rwong1231
rwong1231 over 9 years ago

Hi,

I'm currently having some speed issues that I'm hoping someone might be able to shed some light and recommend/suggest where I might have missed a step? I have a basic SPI setup following Adam Taylor's Microzed(ish) chronicle series 81 - SPI.

In VIVADO:

I've routed the MIO pins to SPI0: SS[0]-MIO13, MOSI-MIO10, MISO-MIO11,SCLK-MIO12.

On the EMIO side, I've routed and constrained the following pins to the JB1 PMOD connector:

** SSI is tied to a constant block (of value 1) in Vivado as suggested in TRM **

SPI0_MOSI_O --> SDO

set_property PACKAGE_PIN Y8 [get_ports SDO]

Y8 is connected to BANK13_LVDS_8_N on the Picozed

SPI0_SCLK_O--> sclk

set_property PACKAGE_PIN W9 [get_ports sclk]

W9 is connected to BANK13_LVDS_9_N on the Picozed

 

In XSDK:

I've duplicated Adam Taylor's _part82.c (via GitHub).

Executing the example code, I'm getting two issues:

A. on the JB1-PL (EMIO) side, I can't go faster than 6.25MHz at the moment. I've tried changing the SPI frequency in Vivado Block Design several times (100MHz, 166.667MHz, 200MHz) and then using XSPIPS_CLK_PRESCALE_32 (or _8, _64 etc..) to fine tune it but still no success.

B. The SPI on JPS1 has no signals coming out. I'm using an oscilloscope to trace the signals at the moment. There are no signals coming out of the Pin 2 and Pin 4 on the JPS1-PMOD connector. (ie..MOSI and SCLK pins).

 

Thank you for any suggestions/recommendations.

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 9 years ago +1 verified
    Hi Nocturnalpea, What is your current Hardware setup(PicoZed 7030/7020/7015/7010 + FMC V2/FMC V1)? Did you complete issue 82 of the SPI setup? Is your main goal with this to implement a SPI design on your…
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Nocturnalpea,

    What is your current Hardware setup(PicoZed 7030/7020/7015/7010 + FMC V2/FMC V1)? Did you complete issue 82 of the SPI setup? Is your main goal with this to implement a SPI design on your hardware? Which version of Vivado are you using?

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • rwong1231
    0 rwong1231 over 9 years ago in reply to jafoste4

    Hi Josh,

    My Hardware setup:

    PicoZed 7020 + FMC V2.

    Software:

    Vivado 2016.4 + XSDK 2016.4

     

    Q: Did you complete issue 82 of the SPI setup?

    Yes. I routed SPI1 through the MIO pins 10-15. And SPI0 via EMIO. In Vivado MIO Configuration menu, it reads:

    SPI1 - MIO10 - mosi

    SPI1 - MIO11 - miso

    SPI1 - MIO12 - sclk

    SPI1 - MIO13 - ss[0]

    image

    For the EMIO, I've applied the constraints as in my original post and routed 'SDO' and 'sclk' out just like Adam. SPI0_SS_I is tied to a constant '1' using the Constant IP. Running the same program Adam provided (ie _part82.c), my EMIO MOSI and SCLK pins have signal. And the output bits is correct using an oscilloscope to read the SDO and sclk pulses. But there's no output on the PSPMOD pins.

    image

     

    Q: Is your main goal with this to implement a SPI design on your hardware?

    Yes. I'll be attaching two SPI-slave devices and the Zynq acting as the master.

     

    Q: Which version of Vivado?

    Vivado 2016.4 and XSDK 2016.4

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rwong1231
    0 rwong1231 over 9 years ago in reply to jafoste4

    Hi Josh,

    My Hardware setup:

    PicoZed 7020 + FMC V2.

    Software:

    Vivado 2016.4 + XSDK 2016.4

     

    Q: Did you complete issue 82 of the SPI setup?

    Yes. I routed SPI1 through the MIO pins 10-15. And SPI0 via EMIO. In Vivado MIO Configuration menu, it reads:

    SPI1 - MIO10 - mosi

    SPI1 - MIO11 - miso

    SPI1 - MIO12 - sclk

    SPI1 - MIO13 - ss[0]

    image

    For the EMIO, I've applied the constraints as in my original post and routed 'SDO' and 'sclk' out just like Adam. SPI0_SS_I is tied to a constant '1' using the Constant IP. Running the same program Adam provided (ie _part82.c), my EMIO MOSI and SCLK pins have signal. And the output bits is correct using an oscilloscope to read the SDO and sclk pulses. But there's no output on the PSPMOD pins.

    image

     

    Q: Is your main goal with this to implement a SPI design on your hardware?

    Yes. I'll be attaching two SPI-slave devices and the Zynq acting as the master.

     

    Q: Which version of Vivado?

    Vivado 2016.4 and XSDK 2016.4