Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Picozed CC Gen2 SPI test - via PS (JPS1) and EMIO (JB1) - slow speeds
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 365 subscribers
  • Views 1439 views
  • Users 0 members are here
Related

Picozed CC Gen2 SPI test - via PS (JPS1) and EMIO (JB1) - slow speeds

rwong1231
rwong1231 over 9 years ago

Hi,

I'm currently having some speed issues that I'm hoping someone might be able to shed some light and recommend/suggest where I might have missed a step? I have a basic SPI setup following Adam Taylor's Microzed(ish) chronicle series 81 - SPI.

In VIVADO:

I've routed the MIO pins to SPI0: SS[0]-MIO13, MOSI-MIO10, MISO-MIO11,SCLK-MIO12.

On the EMIO side, I've routed and constrained the following pins to the JB1 PMOD connector:

** SSI is tied to a constant block (of value 1) in Vivado as suggested in TRM **

SPI0_MOSI_O --> SDO

set_property PACKAGE_PIN Y8 [get_ports SDO]

Y8 is connected to BANK13_LVDS_8_N on the Picozed

SPI0_SCLK_O--> sclk

set_property PACKAGE_PIN W9 [get_ports sclk]

W9 is connected to BANK13_LVDS_9_N on the Picozed

 

In XSDK:

I've duplicated Adam Taylor's _part82.c (via GitHub).

Executing the example code, I'm getting two issues:

A. on the JB1-PL (EMIO) side, I can't go faster than 6.25MHz at the moment. I've tried changing the SPI frequency in Vivado Block Design several times (100MHz, 166.667MHz, 200MHz) and then using XSPIPS_CLK_PRESCALE_32 (or _8, _64 etc..) to fine tune it but still no success.

B. The SPI on JPS1 has no signals coming out. I'm using an oscilloscope to trace the signals at the moment. There are no signals coming out of the Pin 2 and Pin 4 on the JPS1-PMOD connector. (ie..MOSI and SCLK pins).

 

Thank you for any suggestions/recommendations.

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 9 years ago +1 verified
    Hi Nocturnalpea, What is your current Hardware setup(PicoZed 7030/7020/7015/7010 + FMC V2/FMC V1)? Did you complete issue 82 of the SPI setup? Is your main goal with this to implement a SPI design on your…
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi nocturnalpea,

    You may want to downgrade to a 2015 version of the tools as it seems the design was created back in 2015. The reason I make this suggestion is that the SPI drivers may have changed in the last year or so. 

    SPI0 thoughts - I personally havent had much exposure routing through the EMIO so I cannot offer much help on this one, perhaps this is a better question to proposition xilinx on?

    SPI1 thoughts - Your MIO configuration seems to be set up correctly. Looking at https://forums.xilinx.com/t5/Xcell-Daily-Blog/Adam-Taylor-s-MicroZed-ish-Chronicles-Part-82-Simple/ba-p/620899 the first comment by kurtcopley at the bottom may help you get the SPI1 working. 

    If you are interested, I have recently created two SPI reference designs, one targets running the SPI protocol via the PS and the other through the PL of the ZYNQ device on all PicoZed devices. These reference designs are currently unpublished and only updated to Vivado 2016.2. I can send them to you if you would like?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi nocturnalpea,

    You may want to downgrade to a 2015 version of the tools as it seems the design was created back in 2015. The reason I make this suggestion is that the SPI drivers may have changed in the last year or so. 

    SPI0 thoughts - I personally havent had much exposure routing through the EMIO so I cannot offer much help on this one, perhaps this is a better question to proposition xilinx on?

    SPI1 thoughts - Your MIO configuration seems to be set up correctly. Looking at https://forums.xilinx.com/t5/Xcell-Daily-Blog/Adam-Taylor-s-MicroZed-ish-Chronicles-Part-82-Simple/ba-p/620899 the first comment by kurtcopley at the bottom may help you get the SPI1 working. 

    If you are interested, I have recently created two SPI reference designs, one targets running the SPI protocol via the PS and the other through the PL of the ZYNQ device on all PicoZed devices. These reference designs are currently unpublished and only updated to Vivado 2016.2. I can send them to you if you would like?

    --Josh