Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 978 views
  • Users 0 members are here
Related

Xillinux

deaxman
deaxman over 13 years ago

How do I attach anything to PS_GPIO in xillydemo?  It says multiple drivers but what if I want to write HDL code to read in a switch and set an LED?  Both are defined as PS_GPIO  (1 through 7 and 11-18 I think) but if I try to set them I get the conflict becuase they are already used in the xillybus_ins module on line 250ish.  Essentially I just want to know what to do to set a light when I flip a switch with Xillybus.  As it is I can't use any of the ports.  I have tried everything I can think of, including a seperate module that I parameterize in the bottom of xillydemo and feed in the PS_GPIOs as lines.  That approach gives no errors, but it acts as if the module isn't even there.  Thanks a ton in advance for any help!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello,

    As far as I recall, the PS_GPIO lines are governed by Linux' GPIO driver. As such, they are exposed to any user space program as described, for example, here:

    http://falsinsoft.blogspot.co.il/2012/11/access-gpio-from-linux-user-space.html

    But the truth is I never actually used this interface.

    The mapping between the GPIO numbers and their actual pins can be found in the UCF file that goes with the bundle.

    If you want to connect these directly to your logic, just modify the UCF so that your Verilog/VHDL port goes to the desired pin, and assign some dummy pin to the GPIO[..] port.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello,

    As far as I recall, the PS_GPIO lines are governed by Linux' GPIO driver. As such, they are exposed to any user space program as described, for example, here:

    http://falsinsoft.blogspot.co.il/2012/11/access-gpio-from-linux-user-space.html

    But the truth is I never actually used this interface.

    The mapping between the GPIO numbers and their actual pins can be found in the UCF file that goes with the bundle.

    If you want to connect these directly to your logic, just modify the UCF so that your Verilog/VHDL port goes to the desired pin, and assign some dummy pin to the GPIO[..] port.

    Regards,
       Eli