Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 976 views
  • Users 0 members are here
Related

Xillinux

deaxman
deaxman over 13 years ago

How do I attach anything to PS_GPIO in xillydemo?  It says multiple drivers but what if I want to write HDL code to read in a switch and set an LED?  Both are defined as PS_GPIO  (1 through 7 and 11-18 I think) but if I try to set them I get the conflict becuase they are already used in the xillybus_ins module on line 250ish.  Essentially I just want to know what to do to set a light when I flip a switch with Xillybus.  As it is I can't use any of the ports.  I have tried everything I can think of, including a seperate module that I parameterize in the bottom of xillydemo and feed in the PS_GPIOs as lines.  That approach gives no errors, but it acts as if the module isn't even there.  Thanks a ton in advance for any help!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello,

    As far as I recall, the PS_GPIO lines are governed by Linux' GPIO driver. As such, they are exposed to any user space program as described, for example, here:

    http://falsinsoft.blogspot.co.il/2012/11/access-gpio-from-linux-user-space.html

    But the truth is I never actually used this interface.

    The mapping between the GPIO numbers and their actual pins can be found in the UCF file that goes with the bundle.

    If you want to connect these directly to your logic, just modify the UCF so that your Verilog/VHDL port goes to the desired pin, and assign some dummy pin to the GPIO[..] port.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deaxman
    0 deaxman over 13 years ago

    I'll give this a try, what I'm worried about is that xillydemo uses the GPIOs and when I comment the line that takes them in out, it causes an error.  I didn't think to fake the connection and change the pin though, thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deaxman
    0 deaxman over 13 years ago

    dummy ports worked very well, thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to deaxman

    I'm very interested in seeing how you did this? Could you perhaps provide both the VHDL code and the edited ucf file? I would be most grateful!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to deaxman

    Could you please tell me how you used dummy ports, i cant figure it out

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    I'll try to clarify this.

    The situation is usually that you have some signals in your Verilog / VHDL design connected to PMODs, LEDs, buttons or whatever, and they are currently connected to PS_GPIO ports.

    So what I suggest, is to expose those signals on the toplevel module (as inputs, outputs or inouts) just like any FPGA design. Then edit xillydemo.ucf, and assign those signals to the desired physical pins. Again, exactly like a regular FPGA.

    The only problem is that all PS_GPIO signals must be assigned to some physical pin on the device's grid. So the simple solution is to assign them to vacant pins. For example, the FMC connector has a lot of pins that many don't connect to anything, so the PS_GPIO signals that were evicted from their original pin assignments can get just any pin on the FMC connector. Or whatever is free.

    I hope this clarified my point somewhat.

    Regards,
       Eli