Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Booting/InstallingLinux on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 366 subscribers
  • Views 3381 views
  • Users 0 members are here
Related

Booting/InstallingLinux on Zedboard

e14 Contributor
e14 Contributor over 10 years ago

Hi

I am very new with the embedded software world and I am currently trying to boot Linux Kernel on Zedboard from SD CARD. I had about a week back tried to install on a zybo board and it was working. I had followed the same steps but however ended up running into issues. Currently , I am able to connect to the uboot bootup console via usb-uart and the following is the log.

Further details on how I have done this:

1) Obtained the linux uImage

2) Compiled devicetree.dtb from linux-digilent-dev branch

3)Created a base design in Vivado consisting of the processing system and axi gpio. In the Xilinx SDK created a new zyng fsbl(didn't do any changes to any files). 

4) From Xilinx Tools , create boot image i added the systemwrapper.bit , the fsbl. elf and uboot.elf to create boot.bin.

5) Partioned the SD card into 4 mb space left at start, 1 gb fat partition and rest as ext4 partition.

6) Copied the uImage, boot.bin and devicetree.dtb with same names into the 1gb partition.

7) Set JP9 and JP8 to 3V3 amd JP7 ,JP8 and JP11 to GND.

8) Connected the usb-art ,inserted SD card in the slot and powered on.

9) I can see the following output via minicom console.

U-Boot 2014.01 (Aug 09 2016 - 17:17:22)
 
I2C:   ready
Memory: ECC disabled
DRAM:  512 MiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  0 
Configure PL and booting Linux from TFTP...
Device: zynq_sdhci
Manufacturer ID: 3
OEM: 5344
Name: SU04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
Xilinx Device
Descriptor @ 0x1ffbaa54
Family:         Zynq PL
Interface type: Device configuration interface (Zynq)
Device Size:    4045564 bytes
Cookie:         0x20 (32)
Device name:    7z020
No Device Function Table.
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
fpga - loadable FPGA image support
 
Usage:
fpga [operation type] [device number] [image address] [image size]
fpga operations:
  dump  [dev]                   Load device to memory buffer
  info  [dev]                   list known device information
  load  [dev] [address] [size]  Load device from memory buffer
  loadp [dev] [address] [size]  Load device from memory buffer with partial bitstream
  loadb [dev] [address] [size]  Load device from bitstream buffer (Xilinx only)
  loadbp        [dev] [address] [size]  Load device from bitstream buffer with partial bitstream(Xilinx only)
  loadmk [dev] [address]        Load device generated with mkimage
        For loadmk operating on FIT format uImage address must include
        subimage unit name in the form of addr:<subimg_uname>
Load device from filesystem (FAT by default) (Xilinx only)
  loadfs [dev] [address] [image size] [blocksize] <interface>
        [<dev[:part]>] <filename>
 
Gem.e000b000:0 is connected to Gem.e000b000.  Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Gem.e000b000:0 is connected to Gem.e000b000.  Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Gem.e000b000:0 is connected to Gem.e000b000.  Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Wrong Image Format for bootm command
ERROR: can't get kernel image!
zynq-uboot> 
 
The bolded text above has got me wondering why is that it is saying loading from tftp despite i have setup jumpers to boot from sd card? I went to the zynq-common.h bootfile in uboot-digilent-dev-master-next and noticed that if it boots from sd_card the following needs to be done:
 
 
  sdboot=if mmcinfo; then " \
  "run uenvboot; " \
  "echo Copying Linux from SD to RAM... && " \
  "fatload mmc 0 0x3000000 ${kernel_image} && " \
  "fatload mmc 0 0x2A00000 ${devicetree_image} && " \
  "bootm 0x3000000 0x2000000 0x2A00000; " \
  "fi\0" \
   
  so something like copying linux from sd to ram should come up.  Can someone help me with this? I also wanted to know what exactly is being done in the uboot. Has the pl been initialized?
 
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago
    zynq-uboot> printenv
    baudrate=115200
    bitstream_image=system.bit.bin
    boot_image=BOOT.bin
    boot_size=0xF00000
    bootcmd=run $modeboot
    bootdelay=3
    bootenv=uEnv.txt
    devicetree_image=devicetree.dtb
    devicetree_load_address=0x2000000
    devicetree_size=0x20000
    dfu_mmc=run dfu_mmc_info && dfu 0 mmc 0
    dfu_mmc_info=set dfu_alt_info ${kernel_image} fat 0 1\\;${devicetree_image} fat 0 1\\;${ramdisk_image} fat 0 1
    dfu_ram=run dfu_ram_info && dfu 0 ram 0
    dfu_ram_info=set dfu_alt_info ${kernel_image} ram 0x3000000 0x500000\\;${devicetree_image} ram 0x2A00000 0x20000\\;${ramdisk_image} ram 0x2000000 0x600000
    ethact=Gem.e000b000
    ethaddr=00:0a:35:00:01:22
    fdt_high=0x20000000
    importbootenv=echo Importing environment from SD ...; env import -t ${loadbootenv_addr} $filesize
    initrd_high=0x20000000
    ipaddr=192.168.1.4
    jtagboot=echo TFTPing Linux to RAM... && tftpboot ${kernel_load_address} ${kernel_image} && tftpboot ${devicetree_load_address} ${devicetree_image} && tftpboot ${ramdisk_load_address} ${ramdisk_image} && bootm $}
    kernel_image=uImage
    kernel_load_address=0x2080000
    kernel_size=0x500000
    loadbit_addr=0x100000
    loadbootenv=load mmc 0 ${loadbootenv_addr} ${bootenv}
    loadbootenv_addr=0x2000000
    mmc_loadbit=echo Loading bitstream from SD/MMC/eMMC to RAM.. && mmcinfo && load mmc 0 ${loadbit_addr} ${bitstream_image} && fpga load 0 ${loadbit_addr} ${filesize}
    modeboot=sdboot
    nandboot=echo Copying Linux from NAND flash to RAM... && nand read ${kernel_load_address} 0x100000 ${kernel_size} && nand read ${devicetree_load_address} 0x600000 ${devicetree_size} && echo Copying ramdisk... &&}
    norboot=echo Copying Linux from NOR flash to RAM... && cp.b 0xE2100000 ${kernel_load_address} ${kernel_size} && cp.b 0xE2600000 ${devicetree_load_address} ${devicetree_size} && echo Copying ramdisk... && cp.b 0x}
    preboot=if test $modeboot = sdboot && env run sd_uEnvtxt_existence_test; then if env run loadbootenv; then env run importbootenv; fi; fi; 
    qspiboot=echo Copying Linux from QSPI flash to RAM... && sf probe 0 0 0 && sf read ${kernel_load_address} 0x100000 ${kernel_size} && sf read ${devicetree_load_address} 0x600000 ${devicetree_size} && echo Copying}
    ramdisk_image=uramdisk.image.gz
    ramdisk_load_address=0x4000000
    ramdisk_size=0x5E0000
    rsa_jtagboot=echo TFTPing Image to RAM... && tftpboot 0x100000 ${boot_image} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    rsa_nandboot=echo Copying Image from NAND flash to RAM... && nand read 0x100000 0x0 ${boot_size} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    rsa_norboot=echo Copying Image from NOR flash to RAM... && cp.b 0xE2100000 0x100000 ${boot_size} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    rsa_qspiboot=echo Copying Image from QSPI flash to RAM... && sf probe 0 0 0 && sf read 0x100000 0x0 ${boot_size} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_addr}
    rsa_sdboot=echo Copying Image from SD to RAM... && load mmc 0 0x100000 ${boot_image} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    sd_uEnvtxt_existence_test=test -e mmc 0 /uEnv.txt
    sdboot=echo Configure PL and booting Linux from TFTP...;mmcinfo;fpga info 0;tftpboot 0x1000000 system.bin;fpga load 0 0x1000000 3dbafc;tftpboot 0x3000000 ${kernel_image};tftpboot 0x2A00000 ${devicetree_image};tf0
    serverip=192.168.1.20
    stderr=serial
    stdin=serial
    stdout=serial
    thor_mmc=run dfu_mmc_info && thordown 0 mmc 0
    thor_ram=run dfu_ram_info && thordown 0 ram 0
    uenvboot=if run loadbootenv; then echo Loaded environment from ${bootenv}; run importbootenv; fi; if test -n $uenvcmd; then echo Running uenvcmd ...; run uenvcmd; fi
    usbboot=if usb start; then run uenvboot; echo Copying Linux from USB to RAM... && load usb 0 ${kernel_load_address} ${kernel_image} && load usb 0 ${devicetree_load_address} ${devicetree_image} && load usb 0 ${rai
     
    Environment size: 4778/131068 bytes
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago
    zynq-uboot> printenv
    baudrate=115200
    bitstream_image=system.bit.bin
    boot_image=BOOT.bin
    boot_size=0xF00000
    bootcmd=run $modeboot
    bootdelay=3
    bootenv=uEnv.txt
    devicetree_image=devicetree.dtb
    devicetree_load_address=0x2000000
    devicetree_size=0x20000
    dfu_mmc=run dfu_mmc_info && dfu 0 mmc 0
    dfu_mmc_info=set dfu_alt_info ${kernel_image} fat 0 1\\;${devicetree_image} fat 0 1\\;${ramdisk_image} fat 0 1
    dfu_ram=run dfu_ram_info && dfu 0 ram 0
    dfu_ram_info=set dfu_alt_info ${kernel_image} ram 0x3000000 0x500000\\;${devicetree_image} ram 0x2A00000 0x20000\\;${ramdisk_image} ram 0x2000000 0x600000
    ethact=Gem.e000b000
    ethaddr=00:0a:35:00:01:22
    fdt_high=0x20000000
    importbootenv=echo Importing environment from SD ...; env import -t ${loadbootenv_addr} $filesize
    initrd_high=0x20000000
    ipaddr=192.168.1.4
    jtagboot=echo TFTPing Linux to RAM... && tftpboot ${kernel_load_address} ${kernel_image} && tftpboot ${devicetree_load_address} ${devicetree_image} && tftpboot ${ramdisk_load_address} ${ramdisk_image} && bootm $}
    kernel_image=uImage
    kernel_load_address=0x2080000
    kernel_size=0x500000
    loadbit_addr=0x100000
    loadbootenv=load mmc 0 ${loadbootenv_addr} ${bootenv}
    loadbootenv_addr=0x2000000
    mmc_loadbit=echo Loading bitstream from SD/MMC/eMMC to RAM.. && mmcinfo && load mmc 0 ${loadbit_addr} ${bitstream_image} && fpga load 0 ${loadbit_addr} ${filesize}
    modeboot=sdboot
    nandboot=echo Copying Linux from NAND flash to RAM... && nand read ${kernel_load_address} 0x100000 ${kernel_size} && nand read ${devicetree_load_address} 0x600000 ${devicetree_size} && echo Copying ramdisk... &&}
    norboot=echo Copying Linux from NOR flash to RAM... && cp.b 0xE2100000 ${kernel_load_address} ${kernel_size} && cp.b 0xE2600000 ${devicetree_load_address} ${devicetree_size} && echo Copying ramdisk... && cp.b 0x}
    preboot=if test $modeboot = sdboot && env run sd_uEnvtxt_existence_test; then if env run loadbootenv; then env run importbootenv; fi; fi; 
    qspiboot=echo Copying Linux from QSPI flash to RAM... && sf probe 0 0 0 && sf read ${kernel_load_address} 0x100000 ${kernel_size} && sf read ${devicetree_load_address} 0x600000 ${devicetree_size} && echo Copying}
    ramdisk_image=uramdisk.image.gz
    ramdisk_load_address=0x4000000
    ramdisk_size=0x5E0000
    rsa_jtagboot=echo TFTPing Image to RAM... && tftpboot 0x100000 ${boot_image} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    rsa_nandboot=echo Copying Image from NAND flash to RAM... && nand read 0x100000 0x0 ${boot_size} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    rsa_norboot=echo Copying Image from NOR flash to RAM... && cp.b 0xE2100000 0x100000 ${boot_size} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    rsa_qspiboot=echo Copying Image from QSPI flash to RAM... && sf probe 0 0 0 && sf read 0x100000 0x0 ${boot_size} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_addr}
    rsa_sdboot=echo Copying Image from SD to RAM... && load mmc 0 0x100000 ${boot_image} && zynqrsa 0x100000 && bootm ${kernel_load_address} ${ramdisk_load_address} ${devicetree_load_address}
    sd_uEnvtxt_existence_test=test -e mmc 0 /uEnv.txt
    sdboot=echo Configure PL and booting Linux from TFTP...;mmcinfo;fpga info 0;tftpboot 0x1000000 system.bin;fpga load 0 0x1000000 3dbafc;tftpboot 0x3000000 ${kernel_image};tftpboot 0x2A00000 ${devicetree_image};tf0
    serverip=192.168.1.20
    stderr=serial
    stdin=serial
    stdout=serial
    thor_mmc=run dfu_mmc_info && thordown 0 mmc 0
    thor_ram=run dfu_ram_info && thordown 0 ram 0
    uenvboot=if run loadbootenv; then echo Loaded environment from ${bootenv}; run importbootenv; fi; if test -n $uenvcmd; then echo Running uenvcmd ...; run uenvcmd; fi
    usbboot=if usb start; then run uenvboot; echo Copying Linux from USB to RAM... && load usb 0 ${kernel_load_address} ${kernel_image} && load usb 0 ${devicetree_load_address} ${devicetree_image} && load usb 0 ${rai
     
    Environment size: 4778/131068 bytes