Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Booting/InstallingLinux on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 366 subscribers
  • Views 3381 views
  • Users 0 members are here
Related

Booting/InstallingLinux on Zedboard

e14 Contributor
e14 Contributor over 10 years ago

Hi

I am very new with the embedded software world and I am currently trying to boot Linux Kernel on Zedboard from SD CARD. I had about a week back tried to install on a zybo board and it was working. I had followed the same steps but however ended up running into issues. Currently , I am able to connect to the uboot bootup console via usb-uart and the following is the log.

Further details on how I have done this:

1) Obtained the linux uImage

2) Compiled devicetree.dtb from linux-digilent-dev branch

3)Created a base design in Vivado consisting of the processing system and axi gpio. In the Xilinx SDK created a new zyng fsbl(didn't do any changes to any files). 

4) From Xilinx Tools , create boot image i added the systemwrapper.bit , the fsbl. elf and uboot.elf to create boot.bin.

5) Partioned the SD card into 4 mb space left at start, 1 gb fat partition and rest as ext4 partition.

6) Copied the uImage, boot.bin and devicetree.dtb with same names into the 1gb partition.

7) Set JP9 and JP8 to 3V3 amd JP7 ,JP8 and JP11 to GND.

8) Connected the usb-art ,inserted SD card in the slot and powered on.

9) I can see the following output via minicom console.

U-Boot 2014.01 (Aug 09 2016 - 17:17:22)
 
I2C:   ready
Memory: ECC disabled
DRAM:  512 MiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  0 
Configure PL and booting Linux from TFTP...
Device: zynq_sdhci
Manufacturer ID: 3
OEM: 5344
Name: SU04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
Xilinx Device
Descriptor @ 0x1ffbaa54
Family:         Zynq PL
Interface type: Device configuration interface (Zynq)
Device Size:    4045564 bytes
Cookie:         0x20 (32)
Device name:    7z020
No Device Function Table.
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
fpga - loadable FPGA image support
 
Usage:
fpga [operation type] [device number] [image address] [image size]
fpga operations:
  dump  [dev]                   Load device to memory buffer
  info  [dev]                   list known device information
  load  [dev] [address] [size]  Load device from memory buffer
  loadp [dev] [address] [size]  Load device from memory buffer with partial bitstream
  loadb [dev] [address] [size]  Load device from bitstream buffer (Xilinx only)
  loadbp        [dev] [address] [size]  Load device from bitstream buffer with partial bitstream(Xilinx only)
  loadmk [dev] [address]        Load device generated with mkimage
        For loadmk operating on FIT format uImage address must include
        subimage unit name in the form of addr:<subimg_uname>
Load device from filesystem (FAT by default) (Xilinx only)
  loadfs [dev] [address] [image size] [blocksize] <interface>
        [<dev[:part]>] <filename>
 
Gem.e000b000:0 is connected to Gem.e000b000.  Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Gem.e000b000:0 is connected to Gem.e000b000.  Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Gem.e000b000:0 is connected to Gem.e000b000.  Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Wrong Image Format for bootm command
ERROR: can't get kernel image!
zynq-uboot> 
 
The bolded text above has got me wondering why is that it is saying loading from tftp despite i have setup jumpers to boot from sd card? I went to the zynq-common.h bootfile in uboot-digilent-dev-master-next and noticed that if it boots from sd_card the following needs to be done:
 
 
  sdboot=if mmcinfo; then " \
  "run uenvboot; " \
  "echo Copying Linux from SD to RAM... && " \
  "fatload mmc 0 0x3000000 ${kernel_image} && " \
  "fatload mmc 0 0x2A00000 ${devicetree_image} && " \
  "bootm 0x3000000 0x2000000 0x2A00000; " \
  "fi\0" \
   
  so something like copying linux from sd to ram should come up.  Can someone help me with this? I also wanted to know what exactly is being done in the uboot. Has the pl been initialized?
 
  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Andrewmine,

    Take a look at this link http://www.wiki.xilinx.com/Linux 

    Go throught the "System Software Development" steps near the bottom of the screen which details how to build kernel on your system.

    Let me know how that works.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hi

    I have not been able to access that link at all. It says to create an account and I have created the account the day you posted and still haven't been approved yet. I am not sure. However, I have gone through a similar tutorial and reached this stage.

     

    Currently, when I am printing the print env it shows as follows:

     

    sdboot=echo Configure PL and booting Linux from TFTP...;mmcinfo;fpga info 0;tftpboot 0x1000000 system.bin;fpga load 0 0x1000000 3dbafc;tftpboot 0x3000000 ${kernel_image};tftpboot 0x2A00000 ${devicetree_image};tf0
     
     
    which is what the problem is I guess. At the zynq-uboot terminal, when I manually type in the commands :
     
      fatload mmc 0 0x3000000 uImage
      fatload mmc 0 0x2A00000 devicetree.dtb 
      bootm 0x3000000 - 0x2A00000
       
      It works. So my question is why has uboot compiled in such a way and how do I fix it. I have even tried created a uEnv.txt but it is not working as well.
       
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hi

    I have not been able to access that link at all. It says to create an account and I have created the account the day you posted and still haven't been approved yet. I am not sure. However, I have gone through a similar tutorial and reached this stage.

     

    Currently, when I am printing the print env it shows as follows:

     

    sdboot=echo Configure PL and booting Linux from TFTP...;mmcinfo;fpga info 0;tftpboot 0x1000000 system.bin;fpga load 0 0x1000000 3dbafc;tftpboot 0x3000000 ${kernel_image};tftpboot 0x2A00000 ${devicetree_image};tf0
     
     
    which is what the problem is I guess. At the zynq-uboot terminal, when I manually type in the commands :
     
      fatload mmc 0 0x3000000 uImage
      fatload mmc 0 0x2A00000 devicetree.dtb 
      bootm 0x3000000 - 0x2A00000
       
      It works. So my question is why has uboot compiled in such a way and how do I fix it. I have even tried created a uEnv.txt but it is not working as well.