Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Reference Design: Standalone (Bare-Metal) USB Device
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 402 views
  • Users 0 members are here
Related

Reference Design: Standalone (Bare-Metal) USB Device

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone,

I started testing the Standalone USB Device example on a Windows 7 64 Bit-System. Compiling and linking works fine (I use usbps_v_1_05_a instead of usbps_v_1_04_a as mentioned in the tutorial).

When I run the program I get the message from windows, that the device driver could not be installed. Does anyone have an idea what I have to do? Is there necessity for a manual driver installation under windows?

Regards,
Dennis

EDIT: The device manager in Windows says "the device can not be started. (Code 10)"

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 12 years ago

    Hi incubus84,

    Which version of tools are you building this in?

    I went to look at this in Vivado 2013.4 which has a predefined ZedBoard hardware platform containing a definition for usbps_v_1_06_a so I loaded the corresponding usbps_v_1_06_a/example code from the SDK install folder.

    Everything seems to be working for me with these two components in place.  Make sure that the hardware platform you are using has a bsp driver version which matches the usbps_v_1_05_a example.  I accidentally tried usbps_v_1_05_a example code on a usbps_v_1_06_a driver and that did not seem to work as well.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 12 years ago

    Hi incubus84,

    Which version of tools are you building this in?

    I went to look at this in Vivado 2013.4 which has a predefined ZedBoard hardware platform containing a definition for usbps_v_1_06_a so I loaded the corresponding usbps_v_1_06_a/example code from the SDK install folder.

    Everything seems to be working for me with these two components in place.  Make sure that the hardware platform you are using has a bsp driver version which matches the usbps_v_1_05_a example.  I accidentally tried usbps_v_1_05_a example code on a usbps_v_1_06_a driver and that did not seem to work as well.

    Regards,

    -Kevin