Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development LwIP Example UART problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 1063 views
  • Users 0 members are here
Related

LwIP Example UART problem

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I'm new to the ZedBoard and currently I'm trying to run the LwIP examples,
provided by Xilinx, on the Board.
(XAPP1026)

I have connected the USB-JTAG and USB-UART to my host machine.
A Serial Terminal has been configured as always for the ZedBoard.

An Ethernet cable is connecting the ZedBoard and the host machine. The host machine IP configuration is identical to the recommended values in the example.

The Boot Mode Jumper are: PLL Used, JTAG Boot, Cascaded JTAG: MIO[6:2] = 00000.

I've set up the SDK-Project according to the manual, and ran the Software as explained. Hoever, no Serial Terminal output is provided.

There are two things that are not mentioned in the manual, and thus could be the
source of the Problem:
The "fsbl" Project displays an error:

make: *** No rule for Target u00BBC:/PROJECT_FOR_RELEASE/zc702_GigE/HW/project_1/project_1.sdk/design_1_wrapper_hw_platform_0/ps7_init.cu00AB,

The SKD-log displays a warn:

13:57:03 WARNt:  [Hsi 55-1559] Software Design already exists with Name C:PROJECT_FOR_RELEASEzc702_GigEHWproject_1project_1.sdkraw_apps_bspsystem.mss

Has anyone experienced something similar?





  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The link is to a version of XAPP1026 adapted for the ZedBoard that is based on ISE 14.5. If you want to use this project unchanged you will probably need to run it  using the Xilinx ISE tool suite.

     

    If you want to use Vivado then you will need to start with the Xilinx XAPP1026 project and make changes in the project, similar to what was done in the adapted project from the link and the linked forum post, to target the Zedboard and rebuild the project. Also note that the ZedBoard does not have as much DDR memory as the ZC702 board so you may need to change the location of the image.mfs file.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The link is to a version of XAPP1026 adapted for the ZedBoard that is based on ISE 14.5. If you want to use this project unchanged you will probably need to run it  using the Xilinx ISE tool suite.

     

    If you want to use Vivado then you will need to start with the Xilinx XAPP1026 project and make changes in the project, similar to what was done in the adapted project from the link and the linked forum post, to target the Zedboard and rebuild the project. Also note that the ZedBoard does not have as much DDR memory as the ZC702 board so you may need to change the location of the image.mfs file.

     

    -Gary