Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Device tree generation
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 824 views
  • Users 0 members are here
Related

Device tree generation

suppamax
suppamax over 11 years ago

Hi,

I cannot generate a correct DTS for my tests.
I am working with Microzed 7020 and my project consists of PS only.
My dts file is

/dts-v1/;
/ {
t#address-cells = <1>;
t#size-cells = <1>;
tcompatible = "xlnx,zynq-7000";
tmodel = "Xilinx Zynq";
taliases {
ttethernet0 = &ps7_ethernet_0;
ttserial0 = &ps7_uart_1;
ttspi0 = &ps7_qspi_0;
t} ;
tchosen {
ttbootargs = "console=ttyUSB0,115200 root=/dev/ram rw ip=:::::eth0:dhcp earlyprintk";
ttlinux,stdout-path = "/amba@0/serial@e0001000";
t} ;
tcpus {
tt#address-cells = <1>;
tt#size-cells = <0>;
ttps7_cortexa9_0: cpu@0 {
tttbus-handle = <&ps7_axi_interconnect_0>;
tttclock-latency = <1000>;
tttclocks = <&clkc 3>;
tttcompatible = "arm,cortex-a9";
tttdevice_type = "cpu";
tttinterrupt-handle = <&ps7_scugic_0>;
tttoperating-points = <666667 1000000 333334 1000000 222223 1000000>;
tttreg = <0x0>;
tt} ;
ttps7_cortexa9_1: cpu@1 {
tttbus-handle = <&ps7_axi_interconnect_0>;
tttclocks = <&clkc 3>;
tttcompatible = "arm,cortex-a9";
tttdevice_type = "cpu";
tttinterrupt-handle = <&ps7_scugic_0>;
tttreg = <0x1>;
tt} ;
t} ;
tpmu {
ttcompatible = "arm,cortex-a9-pmu";
ttinterrupt-parent = <&ps7_scugic_0>;
ttinterrupts = <0 5 4>, <0 6 4>;
ttreg = <0xf8891000 0x1000>, <0xf8893000 0x1000>;
ttreg-names = "cpu0", "cpu1";
t} ;
tps7_ddr_0: memory@0 {
ttdevice_type = "memory";
ttreg = <0x0 0x40000000>;
t} ;
tps7_axi_interconnect_0: amba@0 {
tt#address-cells = <1>;
tt#size-cells = <1>;
ttcompatible = "xlnx,ps7-axi-interconnect-1.00.a", "simple-bus";
ttranges ;
ttps7_afi_0: ps7-afi@f8008000 {
tttcompatible = "xlnx,ps7-afi-1.00.a";
tttreg = <0xf8008000 0x1000>;
tt} ;
ttps7_afi_1: ps7-afi@f8009000 {
tttcompatible = "xlnx,ps7-afi-1.00.a";
tttreg = <0xf8009000 0x1000>;
tt} ;
ttps7_afi_2: ps7-afi@f800a000 {
tttcompatible = "xlnx,ps7-afi-1.00.a";
tttreg = <0xf800a000 0x1000>;
tt} ;
ttps7_afi_3: ps7-afi@f800b000 {
tttcompatible = "xlnx,ps7-afi-1.00.a";
tttreg = <0xf800b000 0x1000>;
tt} ;
ttps7_clockc_0: ps7-clockc@0 {
tttcompatible = "xlnx,ps7-clockc-1.00.a";
tttxlnx,has-modem = <0x0>;
tttxlnx,input-crystal-freq-hz = <0x1f78a40>;
tt} ;
ttps7_ddrc_0: ps7-ddrc@f8006000 {
tttcompatible = "xlnx,zynq-ddrc-1.0";
tttreg = <0xf8006000 0x1000>;
tttxlnx,has-ecc = <0x0>;
tt} ;
ttps7_dev_cfg_0: ps7-dev-cfg@f8007000 {
tttclock-names = "ref_clk", "fclk0", "fclk1", "fclk2", "fclk3";
tttclocks = <&clkc 12>, <&clkc 15>, <&clkc 16>, <&clkc 17>, <&clkc 18>;
tttcompatible = "xlnx,zynq-devcfg-1.0";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 8 4>;
tttreg = <0xf8007000 0x100>;
tt} ;
ttps7_dma_s: ps7-dma@f8003000 {
ttt#dma-cells = <1>;
ttt#dma-channels = <8>;
ttt#dma-requests = <4>;
tttclock-names = "apb_pclk";
tttclocks = <&clkc 27>;
tttcompatible = "arm,primecell", "arm,pl330";
tttinterrupt-names = "abort", "dma0", "dma1", "dma2", "dma3",
tttt"dma4", "dma5", "dma6", "dma7";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 13 4>, <0 14 4>, <0 15 4>, <0 16 4>, <0 17 4>, <0 40 4>, <0 41 4>, <0 42 4>, <0 43 4>;
tttreg = <0xf8003000 0x1000>;
tt} ;
ttps7_ethernet_0: ps7-ethernet@e000b000 {
ttt#address-cells = <1>;
ttt#size-cells = <0>;
tttclock-names = "ref_clk", "aper_clk";
tttclocks = <&clkc 13>, <&clkc 30>;
tttcompatible = "xlnx,ps7-ethernet-1.00.a";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 22 4>;
tttlocal-mac-address = [00 0a 35 00 00 00];
tttphy-handle = <&phy0>;
tttphy-mode = "rgmii-id";
tttreg = <0xe000b000 0x1000>;
tttxlnx,eth-mode = <0x1>;
tttxlnx,has-mdio = <0x1>;
tttxlnx,ptp-enet-clock = <110000000>;
tttmdio {
tttt#address-cells = <1>;
tttt#size-cells = <0>;
ttttphy0: phy@7 {
tttttcompatible = "marvell,88e1116r";
tttttdevice_type = "ethernet-phy";
tttttreg = <7>;
tttt} ;
ttt} ;
tt} ;
ttps7_globaltimer_0: ps7-globaltimer@f8f00200 {
tttclocks = <&clkc 4>;
tttcompatible = "arm,cortex-a9-global-timer";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <1 11 0x301>;
tttreg = <0xf8f00200 0x100>;
tt} ;
ttps7_gpio_0: ps7-gpio@e000a000 {
ttt#gpio-cells = <2>;
tttclocks = <&clkc 42>;
tttcompatible = "xlnx,zynq-gpio-1.0";
tttemio-gpio-width = <64>;
tttgpio-controller ;
tttgpio-mask-high = <0x0>;
tttgpio-mask-low = <0x5600>;
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 20 4>;
tttreg = <0xe000a000 0x1000>;
tt} ;
ttps7_iop_bus_config_0: ps7-iop-bus-config@e0200000 {
tttcompatible = "xlnx,ps7-iop-bus-config-1.00.a";
tttreg = <0xe0200000 0x1000>;
tt} ;
ttps7_ocmc_0: ps7-ocmc@f800c000 {
tttcompatible = "xlnx,zynq-ocmc-1.0";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 3 4>;
tttreg = <0xf800c000 0x1000>;
tt} ;
ttps7_pl310_0: ps7-pl310@f8f02000 {
tttarm,data-latency = <3 2 2>;
tttarm,tag-latency = <2 2 2>;
tttcache-level = <2>;
tttcache-unified ;
tttcompatible = "arm,pl310-cache";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 2 4>;
tttreg = <0xf8f02000 0x1000>;
tt} ;
ttps7_pmu_0: ps7-pmu@f8891000 {
ttt#address-cells = <1>;
ttt#size-cells = <1>;
tttcompatible = "xlnx,ps7-pmu-1.00.a";
tttranges = <0xf8891000 0xf8891000 0x1000 0xf8893000 0xf8893000 0x1000>;
tt} ;
ttps7_qspi_0: ps7-qspi@e000d000 {
tttclock-names = "ref_clk", "aper_clk";
tttclocks = <&clkc 10>, <&clkc 43>;
tttcompatible = "xlnx,zynq-qspi-1.0";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 19 4>;
tttis-dual = <0>;
tttnum-chip-select = <1>;
tttreg = <0xe000d000 0x1000>;
tttxlnx,fb-clk = <0x1>;
tttxlnx,qspi-mode = <0x0>;
tt} ;
ttps7_qspi_linear_0: ps7-qspi-linear@fc000000 {
tttclock-names = "ref_clk", "aper_clk";
tttclocks = <&clkc 10>, <&clkc 43>;
tttcompatible = "xlnx,ps7-qspi-linear-1.00.a";
tttreg = <0xfc000000 0x1000000>;
tt} ;
ttps7_scugic_0: ps7-scugic@f8f01000 {
ttt#address-cells = <2>;
ttt#interrupt-cells = <3>;
ttt#size-cells = <1>;
tttcompatible = "arm,cortex-a9-gic", "arm,gic";
tttinterrupt-controller ;
tttnum_cpus = <2>;
tttnum_interrupts = <96>;
tttreg = <0xf8f01000 0x1000>, <0xf8f00100 0x100>;
tt} ;
ttps7_scutimer_0: ps7-scutimer@f8f00600 {
tttclocks = <&clkc 4>;
tttcompatible = "arm,cortex-a9-twd-timer";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <1 13 0x301>;
tttreg = <0xf8f00600 0x20>;
tt} ;
ttps7_scuwdt_0: ps7-scuwdt@f8f00620 {
tttclocks = <&clkc 4>;
tttcompatible = "xlnx,ps7-scuwdt-1.00.a";
tttdevice_type = "watchdog";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <1 14 0x301>;
tttreg = <0xf8f00620 0xe0>;
tt} ;
ttps7_sd_0: ps7-sdio@e0100000 {
tttclock-frequency = <51000000>;
tttclock-names = "clk_xin", "clk_ahb";
tttclocks = <&clkc 21>, <&clkc 32>;
tttcompatible = "arasan,sdhci-8.9a";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 24 4>;
tttreg = <0xe0100000 0x1000>;
tttxlnx,has-cd = <0x1>;
tttxlnx,has-power = <0x0>;
tttxlnx,has-wp = <0x1>;
tt} ;
ttps7_slcr_0: ps7-slcr@f8000000 {
ttt#address-cells = <1>;
ttt#size-cells = <1>;
tttcompatible = "xlnx,zynq-slcr", "syscon";
tttranges ;
tttreg = <0xf8000000 0x1000>;
tttclkc: clkc@100 {
tttt#clock-cells = <1>;
ttttclock-output-names = "armpll", "ddrpll", "iopll", "cpu_6or4x", "cpu_3or2x",
ttttt"cpu_2x", "cpu_1x", "ddr2x", "ddr3x", "dci",
ttttt"lqspi", "smc", "pcap", "gem0", "gem1",
ttttt"fclk0", "fclk1", "fclk2", "fclk3", "can0",
ttttt"can1", "sdio0", "sdio1", "uart0", "uart1",
ttttt"spi0", "spi1", "dma", "usb0_aper", "usb1_aper",
ttttt"gem0_aper", "gem1_aper", "sdio0_aper", "sdio1_aper", "spi0_aper",
ttttt"spi1_aper", "can0_aper", "can1_aper", "i2c0_aper", "i2c1_aper",
ttttt"uart0_aper", "uart1_aper", "gpio_aper", "lqspi_aper", "smc_aper",
ttttt"swdt", "dbg_trc", "dbg_apb";
ttttcompatible = "xlnx,ps7-clkc";
ttttfclk-enable = <0xf>;
ttttps-clk-frequency = <33333333>;
ttttreg = <0x100 0x100>;
ttt} ;
tt} ;
ttps7_ttc_0: ps7-ttc@f8001000 {
tttclocks = <&clkc 6>;
tttcompatible = "cdns,ttc";
tttinterrupt-names = "ttc0", "ttc1", "ttc2";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 10 4>, <0 11 4>, <0 12 4>;
tttreg = <0xf8001000 0x1000>;
tt} ;
ttps7_uart_1: serial@e0001000 {
tttclock-names = "ref_clk", "aper_clk";
tttclocks = <&clkc 24>, <&clkc 41>;
tttcompatible = "xlnx,xuartps";
tttcurrent-speed = <115200>;
tttdevice_type = "serial";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 50 4>;
tttport-number = <0>;
tttreg = <0xe0001000 0x1000>;
tttxlnx,has-modem = <0x0>;
tt} ;
ttps7_usb_0: ps7-usb@e0002000 {
tttclocks = <&clkc 28>;
tttcompatible = "xlnx,ps7-usb-1.00.a", "xlnx,zynq-usb-1.00.a";
tttdr_mode = "host";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 21 4>;
tttphy_type = "ulpi";
tttreg = <0xe0002000 0x1000>;
tttusb-reset = <&ps7_gpio_0 7 0>;
tt} ;
ttps7_xadc: ps7-xadc@f8007100 {
tttclocks = <&clkc 12>;
tttcompatible = "xlnx,zynq-xadc-1.00.a";
tttinterrupt-parent = <&ps7_scugic_0>;
tttinterrupts = <0 7 4>;
tttreg = <0xf8007100 0x20>;
tt} ;
t} ;
} ;


and the boot crashes here

## Booting kernel from Legacy Image at 02080000 ...
   Image Name:   Linux-3.18.0-xilinx-06187-gb1d65
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3453304 Bytes = 3.3 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 04000000 ...
   Image Name:  
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    5309954 Bytes = 5.1 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02000000
   Booting using the fdt blob at 0x2000000
   Loading Kernel Image ... OK
   Loading Ramdisk to 1faef000, end 1ffff602 ... OK
   Loading Device Tree to 1faea000, end 1faeec04 ... OK

Starting kernel ...

What am I doing wrong?


Thanks in advance,
Max

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Max,

    Where is your Linux kernel coming from?  Is it something that you built yourself?

    Here is the devicetree that works on my MicroZed:

    /dts-v1/;

    / {
    t#address-cells = <0x1>;
    t#size-cells = <0x1>;
    tcompatible = "xlnx,zynq-zed", "xlnx,zynq-7000";
    tmodel = "Zynq Zed Development Board";

    tchosen {
    ttbootargs = "console=ttyPS0,115200 root=/dev/ram rw earlyprintk";
    ttlinux,stdout-path = "/amba/serial@e0001000";
    t};

    taliases {
    ttethernet0 = "/amba/ethernet@e000b000";
    ttserial0 = "/amba/serial@e0001000";
    ttspi0 = "/amba/spi@e000d000";
    t};

    tmemory {
    ttdevice_type = "memory";
    ttreg = <0x0 0x40000000>;
    t};

    tcpus {
    tt#address-cells = <0x1>;
    tt#size-cells = <0x0>;

    ttcpu@0 {
    tttcompatible = "arm,cortex-a9";
    tttdevice_type = "cpu";
    tttreg = <0x0>;
    tttclocks = <0x1 0x3>;
    tttclock-latency = <0x3e8>;
    tttcpu0-supply = <0x2>;
    tttoperating-points = <0xa2c2b 0xf4240 0x51616 0xf4240>;
    tt};

    ttcpu@1 {
    tttcompatible = "arm,cortex-a9";
    tttdevice_type = "cpu";
    tttreg = <0x1>;
    tttclocks = <0x1 0x3>;
    tt};
    t};

    tpmu {
    ttcompatible = "arm,cortex-a9-pmu";
    ttinterrupts = <0x0 0x5 0x4 0x0 0x6 0x4>;
    ttinterrupt-parent = <0x3>;
    ttreg = <0xf8891000 0x1000 0xf8893000 0x1000>;
    t};

    tfixedregulator@0 {
    ttcompatible = "regulator-fixed";
    ttregulator-name = "VCCPINT";
    ttregulator-min-microvolt = <0xf4240>;
    ttregulator-max-microvolt = <0xf4240>;
    ttregulator-boot-on;
    ttregulator-always-on;
    ttlinux,phandle = <0x2>;
    ttphandle = <0x2>;
    t};

    tamba {
    ttcompatible = "simple-bus";
    tt#address-cells = <0x1>;
    tt#size-cells = <0x1>;
    ttinterrupt-parent = <0x3>;
    ttranges;

    ttadc@f8007100 {
    tttcompatible = "xlnx,zynq-xadc-1.00.a";
    tttreg = <0xf8007100 0x20>;
    tttinterrupts = <0x0 0x7 0x4>;
    tttinterrupt-parent = <0x3>;
    tttclocks = <0x1 0xc>;
    tt};

    ttcan@e0008000 {
    tttcompatible = "xlnx,zynq-can-1.0";
    tttstatus = "disabled";
    tttclocks = <0x1 0x13 0x1 0x24>;
    tttclock-names = "can_clk", "pclk";
    tttreg = <0xe0008000 0x1000>;
    tttinterrupts = <0x0 0x1c 0x4>;
    tttinterrupt-parent = <0x3>;
    ttttx-fifo-depth = <0x40>;
    tttrx-fifo-depth = <0x40>;
    tt};

    ttcan@e0009000 {
    tttcompatible = "xlnx,zynq-can-1.0";
    tttstatus = "disabled";
    tttclocks = <0x1 0x14 0x1 0x25>;
    tttclock-names = "can_clk", "pclk";
    tttreg = <0xe0009000 0x1000>;
    tttinterrupts = <0x0 0x33 0x4>;
    tttinterrupt-parent = <0x3>;
    ttttx-fifo-depth = <0x40>;
    tttrx-fifo-depth = <0x40>;
    tt};

    ttgpio@e000a000 {
    tttcompatible = "xlnx,zynq-gpio-1.0";
    ttt#gpio-cells = <0x2>;
    tttclocks = <0x1 0x2a>;
    tttgpio-controller;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x14 0x4>;
    tttreg = <0xe000a000 0x1000>;
    tt};

    tti2c@e0004000 {
    tttcompatible = "cdns,i2c-r1p10";
    tttstatus = "disabled";
    tttclocks = <0x1 0x26>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x19 0x4>;
    tttreg = <0xe0004000 0x1000>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    tti2c@e0005000 {
    tttcompatible = "cdns,i2c-r1p10";
    tttstatus = "disabled";
    tttclocks = <0x1 0x27>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x30 0x4>;
    tttreg = <0xe0005000 0x1000>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttinterrupt-controller@f8f01000 {
    tttcompatible = "arm,cortex-a9-gic";
    ttt#interrupt-cells = <0x3>;
    tttinterrupt-controller;
    tttreg = <0xf8f01000 0x1000 0xf8f00100 0x100>;
    tttlinux,phandle = <0x3>;
    tttphandle = <0x3>;
    tt};

    ttcache-controller@f8f02000 {
    tttcompatible = "arm,pl310-cache";
    tttreg = <0xf8f02000 0x1000>;
    tttarm,data-latency = <0x3 0x2 0x2>;
    tttarm,tag-latency = <0x2 0x2 0x2>;
    tttcache-unified;
    tttcache-level = <0x2>;
    tt};

    ttmemory-controller@f8006000 {
    tttcompatible = "xlnx,zynq-ddrc-1.0";
    tttreg = <0xf8006000 0x1000>;
    tttxlnx,has-ecc = <0x0>;
    tt};

    ttocmc@f800c000 {
    tttcompatible = "xlnx,zynq-ocmc-1.0";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x3 0x4>;
    tttreg = <0xf800c000 0x1000>;
    tt};

    ttserial@e0000000 {
    tttcompatible = "xlnx,xuartps", "cdns,uart-r1p8";
    tttstatus = "disabled";
    tttclocks = <0x1 0x17 0x1 0x28>;
    tttclock-names = "uart_clk", "pclk";
    tttreg = <0xe0000000 0x1000>;
    tttinterrupts = <0x0 0x1b 0x4>;
    tt};

    ttserial@e0001000 {
    tttcompatible = "xlnx,xuartps", "cdns,uart-r1p8";
    tttstatus = "okay";
    tttclocks = <0x1 0x18 0x1 0x29>;
    tttclock-names = "uart_clk", "pclk";
    tttreg = <0xe0001000 0x1000>;
    tttinterrupts = <0x0 0x32 0x4>;
    tt};

    ttspi@e0006000 {
    tttcompatible = "xlnx,zynq-spi-r1p6";
    tttreg = <0xe0006000 0x1000>;
    tttstatus = "disabled";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x1a 0x4>;
    tttclocks = <0x1 0x19 0x1 0x22>;
    tttclock-names = "ref_clk", "pclk";
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttspi@e0007000 {
    tttcompatible = "xlnx,zynq-spi-r1p6";
    tttreg = <0xe0007000 0x1000>;
    tttstatus = "disabled";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x31 0x4>;
    tttclocks = <0x1 0x1a 0x1 0x23>;
    tttclock-names = "ref_clk", "pclk";
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttspi@e000d000 {
    tttclock-names = "ref_clk", "pclk";
    tttclocks = <0x1 0xa 0x1 0x2b>;
    tttcompatible = "xlnx,zynq-qspi-1.0";
    tttstatus = "okay";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x13 0x4>;
    tttreg = <0xe000d000 0x1000>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tttis-dual = <0x0>;
    tttnum-cs = <0x1>;

    tttflash@0 {
    ttttcompatible = "n25q128a11";
    ttttreg = <0x0>;
    ttttspi-tx-bus-width = <0x1>;
    ttttspi-rx-bus-width = <0x4>;
    ttttspi-max-frequency = <0x2faf080>;
    tttt#address-cells = <0x1>;
    tttt#size-cells = <0x1>;

    ttttpartition@qspi-fsbl-uboot {
    tttttlabel = "qspi-fsbl-uboot";
    tttttreg = <0x0 0x100000>;
    tttt};

    ttttpartition@qspi-linux {
    tttttlabel = "qspi-linux";
    tttttreg = <0x100000 0x500000>;
    tttt};

    ttttpartition@qspi-device-tree {
    tttttlabel = "qspi-device-tree";
    tttttreg = <0x600000 0x20000>;
    tttt};

    ttttpartition@qspi-rootfs {
    tttttlabel = "qspi-rootfs";
    tttttreg = <0x620000 0x5e0000>;
    tttt};

    ttttpartition@qspi-bitstream {
    tttttlabel = "qspi-bitstream";
    tttttreg = <0xc00000 0x400000>;
    tttt};
    ttt};
    tt};

    ttmemory-controller@e000e000 {
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x1>;
    tttstatus = "disabled";
    tttclock-names = "memclk", "aclk";
    tttclocks = <0x1 0xb 0x1 0x2c>;
    tttcompatible = "arm,pl353-smc-r2p1";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x12 0x4>;
    tttranges;
    tttreg = <0xe000e000 0x1000>;

    tttflash@e1000000 {
    ttttstatus = "disabled";
    ttttcompatible = "arm,pl353-nand-r2p1";
    ttttreg = <0xe1000000 0x1000000>;
    tttt#address-cells = <0x1>;
    tttt#size-cells = <0x1>;
    ttt};

    tttflash@e2000000 {
    ttttstatus = "disabled";
    ttttcompatible = "cfi-flash";
    ttttreg = <0xe2000000 0x1000>;
    tttt#address-cells = <0x1>;
    tttt#size-cells = <0x1>;
    ttt};
    tt};

    ttethernet@e000b000 {
    tttcompatible = "xlnx,ps7-ethernet-1.00.a";
    tttreg = <0xe000b000 0x1000>;
    tttstatus = "okay";
    tttinterrupts = <0x0 0x16 0x4>;
    tttclocks = <0x1 0xd 0x1 0x1e>;
    tttclock-names = "ref_clk", "aper_clk";
    tttlocal-mac-address = [00 0a 35 00 00 00];
    tttxlnx,has-mdio = <0x1>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tttphy-mode = "rgmii-id";
    tttphy-handle = <0x4>;

    tttphy@0 {
    ttttreg = <0x0>;
    ttttmarvel,reg-init = <3 16 0xff00 0x1e 3 17 0xfff0 0x00>;
    ttttlinux,phandle = <0x4>;
    ttttphandle = <0x4>;
    ttt};
    tt};

    ttethernet@e000c000 {
    tttcompatible = "xlnx,ps7-ethernet-1.00.a";
    tttreg = <0xe000c000 0x1000>;
    tttstatus = "disabled";
    tttinterrupts = <0x0 0x2d 0x4>;
    tttclocks = <0x1 0xe 0x1 0x1f>;
    tttclock-names = "ref_clk", "aper_clk";
    tttlocal-mac-address = [00 0a 35 00 00 00];
    tttxlnx,has-mdio = <0x1>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttsdhci@e0100000 {
    tttcompatible = "arasan,sdhci-8.9a";
    tttstatus = "okay";
    tttclock-names = "clk_xin", "clk_ahb";
    tttclocks = <0x1 0x15 0x1 0x20>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x18 0x4>;
    tttreg = <0xe0100000 0x1000>;
    tt};

    ttsdhci@e0101000 {
    tttcompatible = "arasan,sdhci-8.9a";
    tttstatus = "disabled";
    tttclock-names = "clk_xin", "clk_ahb";
    tttclocks = <0x1 0x16 0x1 0x21>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x2f 0x4>;
    tttreg = <0xe0101000 0x1000>;
    tt};

    ttslcr@f8000000 {
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x1>;
    tttcompatible = "xlnx,zynq-slcr", "syscon";
    tttreg = <0xf8000000 0x1000>;
    tttranges;

    tttclkc@100 {
    tttt#clock-cells = <0x1>;
    ttttcompatible = "xlnx,ps7-clkc";
    ttttps-clk-frequency = <0x1fca055>;
    ttttfclk-enable = <0xf>;
    ttttclock-output-names = "armpll", "ddrpll", "iopll", "cpu_6or4x", "cpu_3or2x", "cpu_2x", "cpu_1x", "ddr2x", "ddr3x", "dci", "lqspi", "smc", "pcap", "gem0", "gem1", "fclk0", "fclk1", "fclk2", "fclk3", "can0", "can1", "sdio0", "sdio1", "uart0", "uart1", "spi0", "spi1", "dma", "usb0_aper", "usb1_aper", "gem0_aper", "gem1_aper", "sdio0_aper", "sdio1_aper", "spi0_aper", "spi1_aper", "can0_aper", "can1_aper", "i2c0_aper", "i2c1_aper", "uart0_aper", "uart1_aper", "gpio_aper", "lqspi_aper", "smc_aper", "swdt", "dbg_trc", "dbg_apb";
    ttttreg = <0x100 0x100>;
    ttttlinux,phandle = <0x1>;
    ttttphandle = <0x1>;
    ttt};
    tt};

    ttdmac@f8003000 {
    tttcompatible = "arm,pl330", "arm,primecell";
    tttreg = <0xf8003000 0x1000>;
    tttinterrupt-parent = <0x3>;
    tttinterrupt-names = "abort", "dma0", "dma1", "dma2", "dma3", "dma4", "dma5", "dma6", "dma7";
    tttinterrupts = <0x0 0xd 0x4 0x0 0xe 0x4 0x0 0xf 0x4 0x0 0x10 0x4 0x0 0x11 0x4 0x0 0x28 0x4 0x0 0x29 0x4 0x0 0x2a 0x4 0x0 0x2b 0x4>;
    ttt#dma-cells = <0x1>;
    ttt#dma-channels = <0x8>;
    ttt#dma-requests = <0x4>;
    tttclocks = <0x1 0x1b>;
    tttclock-names = "apb_pclk";
    tt};

    ttdevcfg@f8007000 {
    tttclock-names = "ref_clk", "fclk0", "fclk1", "fclk2", "fclk3";
    tttclocks = <0x1 0xc 0x1 0xf 0x1 0x10 0x1 0x11 0x1 0x12>;
    tttcompatible = "xlnx,zynq-devcfg-1.0";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x8 0x4>;
    tttreg = <0xf8007000 0x100>;
    tt};

    tttimer@f8f00200 {
    tttcompatible = "arm,cortex-a9-global-timer";
    tttreg = <0xf8f00200 0x20>;
    tttinterrupts = <0x1 0xb 0x301>;
    tttinterrupt-parent = <0x3>;
    tttclocks = <0x1 0x4>;
    tt};

    tttimer@f8001000 {
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0xa 0x4 0x0 0xb 0x4 0x0 0xc 0x4>;
    tttcompatible = "cdns,ttc";
    tttclocks = <0x1 0x6>;
    tttreg = <0xf8001000 0x1000>;
    tt};

    tttimer@f8002000 {
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x25 0x4 0x0 0x26 0x4 0x0 0x27 0x4>;
    tttcompatible = "cdns,ttc";
    tttclocks = <0x1 0x6>;
    tttreg = <0xf8002000 0x1000>;
    tt};

    tttimer@f8f00600 {
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x1 0xd 0x301>;
    tttcompatible = "arm,cortex-a9-twd-timer";
    tttreg = <0xf8f00600 0x20>;
    tttclocks = <0x1 0x4>;
    tt};

    ttwatchdog@f8005000 {
    tttclocks = <0x1 0x2d>;
    tttcompatible = "xlnx,zynq-wdt-r1p2";
    tttdevice_type = "watchdog";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x9 0x1>;
    tttreg = <0xf8005000 0x1000>;
    tttreset = <0x0>;
    ttttimeout-sec = <0xa>;
    tt};

    ttusb@e0002000 {
    tttclocks = <0x1 0x1c>;
    tttcompatible = "xlnx,ps7-usb-1.00.a", "xlnx,zynq-usb-1.00.a";
    tttstatus = "okay";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x15 0x4>;
    tttreg = <0xe0002000 0x1000>;
    tttdr_mode = "host";
    tttphy_type = "ulpi";
    tt};

    ttusb@e0003000 {
    tttclocks = <0x1 0x1d>;
    tttcompatible = "xlnx,ps7-usb-1.00.a", "xlnx,zynq-usb-1.00.a";
    tttstatus = "disabled";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x2c 0x4>;
    tttreg = <0xe0003000 0x1000>;
    tt};
    t};
    };



    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Max,

    Where is your Linux kernel coming from?  Is it something that you built yourself?

    Here is the devicetree that works on my MicroZed:

    /dts-v1/;

    / {
    t#address-cells = <0x1>;
    t#size-cells = <0x1>;
    tcompatible = "xlnx,zynq-zed", "xlnx,zynq-7000";
    tmodel = "Zynq Zed Development Board";

    tchosen {
    ttbootargs = "console=ttyPS0,115200 root=/dev/ram rw earlyprintk";
    ttlinux,stdout-path = "/amba/serial@e0001000";
    t};

    taliases {
    ttethernet0 = "/amba/ethernet@e000b000";
    ttserial0 = "/amba/serial@e0001000";
    ttspi0 = "/amba/spi@e000d000";
    t};

    tmemory {
    ttdevice_type = "memory";
    ttreg = <0x0 0x40000000>;
    t};

    tcpus {
    tt#address-cells = <0x1>;
    tt#size-cells = <0x0>;

    ttcpu@0 {
    tttcompatible = "arm,cortex-a9";
    tttdevice_type = "cpu";
    tttreg = <0x0>;
    tttclocks = <0x1 0x3>;
    tttclock-latency = <0x3e8>;
    tttcpu0-supply = <0x2>;
    tttoperating-points = <0xa2c2b 0xf4240 0x51616 0xf4240>;
    tt};

    ttcpu@1 {
    tttcompatible = "arm,cortex-a9";
    tttdevice_type = "cpu";
    tttreg = <0x1>;
    tttclocks = <0x1 0x3>;
    tt};
    t};

    tpmu {
    ttcompatible = "arm,cortex-a9-pmu";
    ttinterrupts = <0x0 0x5 0x4 0x0 0x6 0x4>;
    ttinterrupt-parent = <0x3>;
    ttreg = <0xf8891000 0x1000 0xf8893000 0x1000>;
    t};

    tfixedregulator@0 {
    ttcompatible = "regulator-fixed";
    ttregulator-name = "VCCPINT";
    ttregulator-min-microvolt = <0xf4240>;
    ttregulator-max-microvolt = <0xf4240>;
    ttregulator-boot-on;
    ttregulator-always-on;
    ttlinux,phandle = <0x2>;
    ttphandle = <0x2>;
    t};

    tamba {
    ttcompatible = "simple-bus";
    tt#address-cells = <0x1>;
    tt#size-cells = <0x1>;
    ttinterrupt-parent = <0x3>;
    ttranges;

    ttadc@f8007100 {
    tttcompatible = "xlnx,zynq-xadc-1.00.a";
    tttreg = <0xf8007100 0x20>;
    tttinterrupts = <0x0 0x7 0x4>;
    tttinterrupt-parent = <0x3>;
    tttclocks = <0x1 0xc>;
    tt};

    ttcan@e0008000 {
    tttcompatible = "xlnx,zynq-can-1.0";
    tttstatus = "disabled";
    tttclocks = <0x1 0x13 0x1 0x24>;
    tttclock-names = "can_clk", "pclk";
    tttreg = <0xe0008000 0x1000>;
    tttinterrupts = <0x0 0x1c 0x4>;
    tttinterrupt-parent = <0x3>;
    ttttx-fifo-depth = <0x40>;
    tttrx-fifo-depth = <0x40>;
    tt};

    ttcan@e0009000 {
    tttcompatible = "xlnx,zynq-can-1.0";
    tttstatus = "disabled";
    tttclocks = <0x1 0x14 0x1 0x25>;
    tttclock-names = "can_clk", "pclk";
    tttreg = <0xe0009000 0x1000>;
    tttinterrupts = <0x0 0x33 0x4>;
    tttinterrupt-parent = <0x3>;
    ttttx-fifo-depth = <0x40>;
    tttrx-fifo-depth = <0x40>;
    tt};

    ttgpio@e000a000 {
    tttcompatible = "xlnx,zynq-gpio-1.0";
    ttt#gpio-cells = <0x2>;
    tttclocks = <0x1 0x2a>;
    tttgpio-controller;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x14 0x4>;
    tttreg = <0xe000a000 0x1000>;
    tt};

    tti2c@e0004000 {
    tttcompatible = "cdns,i2c-r1p10";
    tttstatus = "disabled";
    tttclocks = <0x1 0x26>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x19 0x4>;
    tttreg = <0xe0004000 0x1000>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    tti2c@e0005000 {
    tttcompatible = "cdns,i2c-r1p10";
    tttstatus = "disabled";
    tttclocks = <0x1 0x27>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x30 0x4>;
    tttreg = <0xe0005000 0x1000>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttinterrupt-controller@f8f01000 {
    tttcompatible = "arm,cortex-a9-gic";
    ttt#interrupt-cells = <0x3>;
    tttinterrupt-controller;
    tttreg = <0xf8f01000 0x1000 0xf8f00100 0x100>;
    tttlinux,phandle = <0x3>;
    tttphandle = <0x3>;
    tt};

    ttcache-controller@f8f02000 {
    tttcompatible = "arm,pl310-cache";
    tttreg = <0xf8f02000 0x1000>;
    tttarm,data-latency = <0x3 0x2 0x2>;
    tttarm,tag-latency = <0x2 0x2 0x2>;
    tttcache-unified;
    tttcache-level = <0x2>;
    tt};

    ttmemory-controller@f8006000 {
    tttcompatible = "xlnx,zynq-ddrc-1.0";
    tttreg = <0xf8006000 0x1000>;
    tttxlnx,has-ecc = <0x0>;
    tt};

    ttocmc@f800c000 {
    tttcompatible = "xlnx,zynq-ocmc-1.0";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x3 0x4>;
    tttreg = <0xf800c000 0x1000>;
    tt};

    ttserial@e0000000 {
    tttcompatible = "xlnx,xuartps", "cdns,uart-r1p8";
    tttstatus = "disabled";
    tttclocks = <0x1 0x17 0x1 0x28>;
    tttclock-names = "uart_clk", "pclk";
    tttreg = <0xe0000000 0x1000>;
    tttinterrupts = <0x0 0x1b 0x4>;
    tt};

    ttserial@e0001000 {
    tttcompatible = "xlnx,xuartps", "cdns,uart-r1p8";
    tttstatus = "okay";
    tttclocks = <0x1 0x18 0x1 0x29>;
    tttclock-names = "uart_clk", "pclk";
    tttreg = <0xe0001000 0x1000>;
    tttinterrupts = <0x0 0x32 0x4>;
    tt};

    ttspi@e0006000 {
    tttcompatible = "xlnx,zynq-spi-r1p6";
    tttreg = <0xe0006000 0x1000>;
    tttstatus = "disabled";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x1a 0x4>;
    tttclocks = <0x1 0x19 0x1 0x22>;
    tttclock-names = "ref_clk", "pclk";
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttspi@e0007000 {
    tttcompatible = "xlnx,zynq-spi-r1p6";
    tttreg = <0xe0007000 0x1000>;
    tttstatus = "disabled";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x31 0x4>;
    tttclocks = <0x1 0x1a 0x1 0x23>;
    tttclock-names = "ref_clk", "pclk";
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttspi@e000d000 {
    tttclock-names = "ref_clk", "pclk";
    tttclocks = <0x1 0xa 0x1 0x2b>;
    tttcompatible = "xlnx,zynq-qspi-1.0";
    tttstatus = "okay";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x13 0x4>;
    tttreg = <0xe000d000 0x1000>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tttis-dual = <0x0>;
    tttnum-cs = <0x1>;

    tttflash@0 {
    ttttcompatible = "n25q128a11";
    ttttreg = <0x0>;
    ttttspi-tx-bus-width = <0x1>;
    ttttspi-rx-bus-width = <0x4>;
    ttttspi-max-frequency = <0x2faf080>;
    tttt#address-cells = <0x1>;
    tttt#size-cells = <0x1>;

    ttttpartition@qspi-fsbl-uboot {
    tttttlabel = "qspi-fsbl-uboot";
    tttttreg = <0x0 0x100000>;
    tttt};

    ttttpartition@qspi-linux {
    tttttlabel = "qspi-linux";
    tttttreg = <0x100000 0x500000>;
    tttt};

    ttttpartition@qspi-device-tree {
    tttttlabel = "qspi-device-tree";
    tttttreg = <0x600000 0x20000>;
    tttt};

    ttttpartition@qspi-rootfs {
    tttttlabel = "qspi-rootfs";
    tttttreg = <0x620000 0x5e0000>;
    tttt};

    ttttpartition@qspi-bitstream {
    tttttlabel = "qspi-bitstream";
    tttttreg = <0xc00000 0x400000>;
    tttt};
    ttt};
    tt};

    ttmemory-controller@e000e000 {
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x1>;
    tttstatus = "disabled";
    tttclock-names = "memclk", "aclk";
    tttclocks = <0x1 0xb 0x1 0x2c>;
    tttcompatible = "arm,pl353-smc-r2p1";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x12 0x4>;
    tttranges;
    tttreg = <0xe000e000 0x1000>;

    tttflash@e1000000 {
    ttttstatus = "disabled";
    ttttcompatible = "arm,pl353-nand-r2p1";
    ttttreg = <0xe1000000 0x1000000>;
    tttt#address-cells = <0x1>;
    tttt#size-cells = <0x1>;
    ttt};

    tttflash@e2000000 {
    ttttstatus = "disabled";
    ttttcompatible = "cfi-flash";
    ttttreg = <0xe2000000 0x1000>;
    tttt#address-cells = <0x1>;
    tttt#size-cells = <0x1>;
    ttt};
    tt};

    ttethernet@e000b000 {
    tttcompatible = "xlnx,ps7-ethernet-1.00.a";
    tttreg = <0xe000b000 0x1000>;
    tttstatus = "okay";
    tttinterrupts = <0x0 0x16 0x4>;
    tttclocks = <0x1 0xd 0x1 0x1e>;
    tttclock-names = "ref_clk", "aper_clk";
    tttlocal-mac-address = [00 0a 35 00 00 00];
    tttxlnx,has-mdio = <0x1>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tttphy-mode = "rgmii-id";
    tttphy-handle = <0x4>;

    tttphy@0 {
    ttttreg = <0x0>;
    ttttmarvel,reg-init = <3 16 0xff00 0x1e 3 17 0xfff0 0x00>;
    ttttlinux,phandle = <0x4>;
    ttttphandle = <0x4>;
    ttt};
    tt};

    ttethernet@e000c000 {
    tttcompatible = "xlnx,ps7-ethernet-1.00.a";
    tttreg = <0xe000c000 0x1000>;
    tttstatus = "disabled";
    tttinterrupts = <0x0 0x2d 0x4>;
    tttclocks = <0x1 0xe 0x1 0x1f>;
    tttclock-names = "ref_clk", "aper_clk";
    tttlocal-mac-address = [00 0a 35 00 00 00];
    tttxlnx,has-mdio = <0x1>;
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x0>;
    tt};

    ttsdhci@e0100000 {
    tttcompatible = "arasan,sdhci-8.9a";
    tttstatus = "okay";
    tttclock-names = "clk_xin", "clk_ahb";
    tttclocks = <0x1 0x15 0x1 0x20>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x18 0x4>;
    tttreg = <0xe0100000 0x1000>;
    tt};

    ttsdhci@e0101000 {
    tttcompatible = "arasan,sdhci-8.9a";
    tttstatus = "disabled";
    tttclock-names = "clk_xin", "clk_ahb";
    tttclocks = <0x1 0x16 0x1 0x21>;
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x2f 0x4>;
    tttreg = <0xe0101000 0x1000>;
    tt};

    ttslcr@f8000000 {
    ttt#address-cells = <0x1>;
    ttt#size-cells = <0x1>;
    tttcompatible = "xlnx,zynq-slcr", "syscon";
    tttreg = <0xf8000000 0x1000>;
    tttranges;

    tttclkc@100 {
    tttt#clock-cells = <0x1>;
    ttttcompatible = "xlnx,ps7-clkc";
    ttttps-clk-frequency = <0x1fca055>;
    ttttfclk-enable = <0xf>;
    ttttclock-output-names = "armpll", "ddrpll", "iopll", "cpu_6or4x", "cpu_3or2x", "cpu_2x", "cpu_1x", "ddr2x", "ddr3x", "dci", "lqspi", "smc", "pcap", "gem0", "gem1", "fclk0", "fclk1", "fclk2", "fclk3", "can0", "can1", "sdio0", "sdio1", "uart0", "uart1", "spi0", "spi1", "dma", "usb0_aper", "usb1_aper", "gem0_aper", "gem1_aper", "sdio0_aper", "sdio1_aper", "spi0_aper", "spi1_aper", "can0_aper", "can1_aper", "i2c0_aper", "i2c1_aper", "uart0_aper", "uart1_aper", "gpio_aper", "lqspi_aper", "smc_aper", "swdt", "dbg_trc", "dbg_apb";
    ttttreg = <0x100 0x100>;
    ttttlinux,phandle = <0x1>;
    ttttphandle = <0x1>;
    ttt};
    tt};

    ttdmac@f8003000 {
    tttcompatible = "arm,pl330", "arm,primecell";
    tttreg = <0xf8003000 0x1000>;
    tttinterrupt-parent = <0x3>;
    tttinterrupt-names = "abort", "dma0", "dma1", "dma2", "dma3", "dma4", "dma5", "dma6", "dma7";
    tttinterrupts = <0x0 0xd 0x4 0x0 0xe 0x4 0x0 0xf 0x4 0x0 0x10 0x4 0x0 0x11 0x4 0x0 0x28 0x4 0x0 0x29 0x4 0x0 0x2a 0x4 0x0 0x2b 0x4>;
    ttt#dma-cells = <0x1>;
    ttt#dma-channels = <0x8>;
    ttt#dma-requests = <0x4>;
    tttclocks = <0x1 0x1b>;
    tttclock-names = "apb_pclk";
    tt};

    ttdevcfg@f8007000 {
    tttclock-names = "ref_clk", "fclk0", "fclk1", "fclk2", "fclk3";
    tttclocks = <0x1 0xc 0x1 0xf 0x1 0x10 0x1 0x11 0x1 0x12>;
    tttcompatible = "xlnx,zynq-devcfg-1.0";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x8 0x4>;
    tttreg = <0xf8007000 0x100>;
    tt};

    tttimer@f8f00200 {
    tttcompatible = "arm,cortex-a9-global-timer";
    tttreg = <0xf8f00200 0x20>;
    tttinterrupts = <0x1 0xb 0x301>;
    tttinterrupt-parent = <0x3>;
    tttclocks = <0x1 0x4>;
    tt};

    tttimer@f8001000 {
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0xa 0x4 0x0 0xb 0x4 0x0 0xc 0x4>;
    tttcompatible = "cdns,ttc";
    tttclocks = <0x1 0x6>;
    tttreg = <0xf8001000 0x1000>;
    tt};

    tttimer@f8002000 {
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x25 0x4 0x0 0x26 0x4 0x0 0x27 0x4>;
    tttcompatible = "cdns,ttc";
    tttclocks = <0x1 0x6>;
    tttreg = <0xf8002000 0x1000>;
    tt};

    tttimer@f8f00600 {
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x1 0xd 0x301>;
    tttcompatible = "arm,cortex-a9-twd-timer";
    tttreg = <0xf8f00600 0x20>;
    tttclocks = <0x1 0x4>;
    tt};

    ttwatchdog@f8005000 {
    tttclocks = <0x1 0x2d>;
    tttcompatible = "xlnx,zynq-wdt-r1p2";
    tttdevice_type = "watchdog";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x9 0x1>;
    tttreg = <0xf8005000 0x1000>;
    tttreset = <0x0>;
    ttttimeout-sec = <0xa>;
    tt};

    ttusb@e0002000 {
    tttclocks = <0x1 0x1c>;
    tttcompatible = "xlnx,ps7-usb-1.00.a", "xlnx,zynq-usb-1.00.a";
    tttstatus = "okay";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x15 0x4>;
    tttreg = <0xe0002000 0x1000>;
    tttdr_mode = "host";
    tttphy_type = "ulpi";
    tt};

    ttusb@e0003000 {
    tttclocks = <0x1 0x1d>;
    tttcompatible = "xlnx,ps7-usb-1.00.a", "xlnx,zynq-usb-1.00.a";
    tttstatus = "disabled";
    tttinterrupt-parent = <0x3>;
    tttinterrupts = <0x0 0x2c 0x4>;
    tttreg = <0xe0003000 0x1000>;
    tt};
    t};
    };



    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • suppamax
    0 suppamax over 11 years ago in reply to zedhed

    Hi Kevin,

    with your devicetree I can boot linux: could you please tell me which procedure to follow for a correct devicetree generation? I followed this http://www.wiki.xilinx.com/Build+Device+Tree+Blob but without success so far.

    With yout DT I cannot use eth

    zynq> ifconfig eth0 192.168.1.115
    xemacps e000b000.ethernet: eth0: no PHY found
    xemacps e000b000.ethernet: XEMACPS mii bus mii_probe fail.
    ifconfig: SIOCSIFFLAGS: No such device or address

    Is this expected?


    Thanks for your help,
    Max

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 11 years ago in reply to suppamax

    Hi Max,

    To be honest, I have never successfully used the devicetree generator outside the PetaLinux toolflow.

    You might call me stubborn, but if I am not using PetaLinux, I usually just start with a known good ZC702 or ZedBoard devicetree and hand modify it to fit the application that I am working on.

    The error message you show is not expected.  I have two suggestions on where to check next.

    1)  Make sure that GEM0 is enabled in your hardware platform PS7 configuration.  If the hardware is not enabled in the hardware platform, the driver will not be able to see a PHY attached to it.

    2)  If you insist on using a kernel you built yourself, check that you are using a known good kernel release tag and not just the HEAD of the repository.  I will post some more in the other response below.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • suppamax
    0 suppamax over 11 years ago in reply to zedhed

    Regarding point 1)
    Eth works, because u-boot downloads the linux image and devicetree via tftp. Is this enough to say that GEM0 is enabled or not?