Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development VGA  on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 365 subscribers
  • Views 2654 views
  • Users 0 members are here
Related

VGA  on Zedboard

e14 Contributor
e14 Contributor over 14 years ago

Hi all, I am a fan of the Zedboard. And fortunately I got one.

But I found it was difficulty for me to play this board.

I just want how to control the VGA under the linux attached in the Zedboard.

I saw a VGA demo on the Zedboard that can showed a Digilent logo through VGA. And I knew that this demo was implemented through the PL only.

I want to know if I can control the VGA using the C program language under the Linux porting in the Zedboard and how I can done this.

And did anyone know how the demos were implemented? Could I get the source project files about these demos?

And were there any other forums that contained the projects about Zedboard? Cause I found there was very few information about on the Internet.

I am appreciative for any information.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    VGA port on Zedboard can only be controlled from the PL logic.  To control the VGA port you will need an AXI bus master controller that generate VGA scan signal from DDR memory. 
    To control the VGA display controller from Linux, a frame buffer device driver is needed to drive the display device.
    Xylon has a display controller solution for Zynq chip. 
    And here is some information about creating a simple Vedio generator on FPGA: http://www.fpga4fun.com/PongGame.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    VGA port on Zedboard can only be controlled from the PL logic.  To control the VGA port you will need an AXI bus master controller that generate VGA scan signal from DDR memory. 
    To control the VGA display controller from Linux, a frame buffer device driver is needed to drive the display device.
    Xylon has a display controller solution for Zynq chip. 
    And here is some information about creating a simple Vedio generator on FPGA: http://www.fpga4fun.com/PongGame.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I think the easiest way is to create framebuffer by using AXI connections. Meaby need some line buffer.
    VGA is only 8bit so 800x600 takes about 470 kB so this can be stored to DDR. Slave AXI can take Framebuffer address and use master AXI to read framebuffer from DDR.


    Then you only need to write drivers for linux and configure to X using it or use direct memory access to that area.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for your reply!

    One more question.
    In the Technical Reference Manual, I found "Configure MIO pin 46 for the RxD signal . Write  0x0000_12E1  to the slcr.MIO_PIN_46 register".

    I just wanted to know why the 0x0000_12E1 corresponds to the RxD singal. I searched the characters "0x0000_12E1" in the TRM file, but no results returned. So these must no be any information about the mapping relationships between the IO singal and its vaules, such as the RxD singal correspondding to the "0x0000_12E1".

    So where can I find the IO signal mapping relationshios?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    parallelcell,

    Would you mind posting this question as a separate thread?  It has nothing to do with your original question, and prevents the community from seeing it.

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    ok