Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Xillinux issue with startx
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 363 subscribers
  • Views 1251 views
  • Users 0 members are here
Related

Xillinux issue with startx

e14 Contributor
e14 Contributor over 14 years ago

I have tried the Xillinux example with Ubuntu
I get the login right, but when I try startx i get the following error:

root@localhost:~# startx
hostname: Name or service not known
xauth: (stdin):1:  bad display name "localhost.localdomain:0" in "add" command


X.Org X Server 1.11.3
Release Date: 2011-12-16
X Protocol Version 11, Revision 0
Build Operating System: Linux 2.6.38-1209-omap4 armv7l Ubuntu
Current Operating System: Linux localhost.localdomain 3.3.0-xillinux-1.0+ #2 SMP PREEMPT Wed Oct 17 17:09:20 IST 2012 armv7l
Kernel command line: consoleblank=0 root=/dev/mmcblk0p2 rw rootwait earlyprintk
Build Date: 05 April 2012  12:04:28AM
xorg-server 2:1.11.4-0ubuntu10 (For technical support please see http://www.ubuntu.com/support)
Current version of pixman: 0.24.4
        Before reporting problems, check http://wiki.x.org
        to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
        (++) from command line, (!!) notice, (II) informational,
        (WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/var/log/Xorg.0.log", Time: Thu Jan  1 00:14:24 1970
(==) Using system config directory "/usr/share/X11/xorg.conf.d"
Parse error on line 2 of section (null) in file /usr/share/X11/xorg.conf.d/10-evdev.conf
        "
         5u00A7
          (
           " is not a valid keyword in this section.
(EE) Problem parsing the config file
(EE) Error parsing the config file

Fatal server error:
no screens found

Please consult the The X.Org Foundation support
         at http://wiki.x.org
for help.
Please also check the log file at "/var/log/Xorg.0.log" for additional information.

ddxSigGiveUp: Closing log
Server terminated with error (1). Closing log file.
xinit: giving up
xinit: unable to connect to X server: No such file or directory
xinit: server error
xauth: (argv):1:  bad display name "localhost.localdomain:0" in "remove" command
root@localhost:~#

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    First of all, did you attempt to run "startx" from the serial console? I don't think that's supposed to work. The command should be issued from a keyboard connected to the Zedboard.

    Otherwise, the reasonable explanation for a failure like this is that some file was damaged during an unclean powerdown of the board. The quickest fix is to rewrite the image to the the SD card.

    It's pointless to debug problems like this. Since all systems start with exactly the same hardware configuration and software image, they should work exactly the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    First of all, did you attempt to run "startx" from the serial console? I don't think that's supposed to work. The command should be issued from a keyboard connected to the Zedboard.

    Otherwise, the reasonable explanation for a failure like this is that some file was damaged during an unclean powerdown of the board. The quickest fix is to rewrite the image to the the SD card.

    It's pointless to debug problems like this. Since all systems start with exactly the same hardware configuration and software image, they should work exactly the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I was able to solve it. Issue was on the USB to SD card writer who was ramdonly writing wrong parts of the SD. Changed SD and everything was fine.

    regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Hello!

    Sometimes I starting to get many IO errors during startup or shutting down.

    It looks like :
    "
    mmcblk0: error -110 transferring data, sector xx, nr 8, cmd responce 0x900, card status 0xc00
    end_request: I/O error, dev mmcblk0,  sector xx
    "
    screenshot - http://imageshack.us/photo/my-images/402/13112012007.jpg/

    After that startx became fails to start. Helps only recovering original image to SD card.

    What is going wrong ? Is there not enough speed or size of SD card (I used SD card which was included with ZedBoard) ?

    thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I am using a SanDisk SDHC Card class 4 with no issues at all

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Got the same problem, however I think it does not really affect system performance? Have you had any problems except error messages? My system produces them sometimes... However I feel it is mainly during big write-operations this happens. Is this your case as well?

    You could also try to start with the zedboard reading rootfs from USB flash drive, works like a charm! ;)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    The problem you report is exactly what a low-quality SD card produces. It simply fails on some sectors. The question is not why it doesn't work, but how come people manage to boot anything from it.

    Please get yourself a Sandisk card, and play around happily ever after. :)