Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development USB Driver (Bare-Metal)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1011 views
  • Users 0 members are here
Related

USB Driver (Bare-Metal)

julian-bauer
julian-bauer over 9 years ago

Hello,

Is there a way to use USB in bare-metal without using Linux?

The Application should be able to write Data (in a stream) to a mass-storage drive via USB.

Using Linux + bare-metal as a AMP-solution would be to complicate in my opinion.

Thank you,

Julian

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 9 years ago +1
    Hi Julian, Please refer to this post http://zedboard.org/content/usb-storage-using-bare-metal-application-zedboard --Josh
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Julian,

    Please refer to this post

    http://zedboard.org/content/usb-storage-using-bare-metal-application-zedboard

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • julian-bauer
    0 julian-bauer over 9 years ago in reply to jafoste4

    Hi Josh,

    i know that the standalone driver supports only device mode functionality, but this is jsut a driver thing, isn't it? it should be possible to initialize the usb port as host, because linux does the same. 

     

    at the moment i try to implement xapp1078 with petalinux on core0 and ethernet lwip on core1 but there is a problem with the lwip ethernet hardware driver. everything works correct without petalinux. together i cant send TCP, it stucks after ARP protocol...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 9 years ago

    Hi there,

    Is your Petalinux install controlling the Ethernet MAC?  If that is the case, you probably cannot access that hardware through the LWIP instance.

    As for trying to use the USB on baremetal as a HOST, there is a LOT of overhead that Linux takes care of.  If you are dead set on trying this for the reason of using two ethernets and NOT utilizing a second MAC in the PL, I would suggest trying to use the USB under the Petalinux and provide the hardware MAC to the LWIP install.

    That aside, I would suggest adding a second MAC and PHY, using whatever expansion your board has.  If it is FMC you can leverage something from Opsero.

    --Dan