Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development USB Driver (Bare-Metal)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1012 views
  • Users 0 members are here
Related

USB Driver (Bare-Metal)

julian-bauer
julian-bauer over 9 years ago

Hello,

Is there a way to use USB in bare-metal without using Linux?

The Application should be able to write Data (in a stream) to a mass-storage drive via USB.

Using Linux + bare-metal as a AMP-solution would be to complicate in my opinion.

Thank you,

Julian

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 9 years ago +1
    Hi Julian, Please refer to this post http://zedboard.org/content/usb-storage-using-bare-metal-application-zedboard --Josh
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Julian,

    Please refer to this post

    http://zedboard.org/content/usb-storage-using-bare-metal-application-zedboard

    --Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • julian-bauer
    0 julian-bauer over 9 years ago in reply to jafoste4

    Hi Josh,

    i know that the standalone driver supports only device mode functionality, but this is jsut a driver thing, isn't it? it should be possible to initialize the usb port as host, because linux does the same. 

     

    at the moment i try to implement xapp1078 with petalinux on core0 and ethernet lwip on core1 but there is a problem with the lwip ethernet hardware driver. everything works correct without petalinux. together i cant send TCP, it stucks after ARP protocol...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • julian-bauer
    0 julian-bauer over 9 years ago in reply to jafoste4

    Hi Josh,

    i know that the standalone driver supports only device mode functionality, but this is jsut a driver thing, isn't it? it should be possible to initialize the usb port as host, because linux does the same. 

     

    at the moment i try to implement xapp1078 with petalinux on core0 and ethernet lwip on core1 but there is a problem with the lwip ethernet hardware driver. everything works correct without petalinux. together i cant send TCP, it stucks after ARP protocol...