Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PS I2C ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 1738 views
  • Users 0 members are here
Related

PS I2C ZedBoard

e14 Contributor
e14 Contributor over 12 years ago

I am trying to get the I2C 0 Peripheral to work on the ZedBoard. I have set up I2C 0 to connect the MIO10 and MIO11 pins to the PMOD header. I then built the linux kernel using the linux-xlnx git source. When in linux any command that is used on the i2c times out.

The following are console outputs:

zynq> i2cdetect -l 0
i2c-0   i2c             XILINX I2C at e0004000            I2C adapter


zynq> i2cdetect 0
Error: Can't use SMBus Quick Write command on this bus

zynq> i2cdetect -r 0
WARNING! This program can confuse your I2C bus, cause data loss and worse!
I will probe file /dev/i2c-0 using read byte commands.
I will probe address range 0x03-0x77.
Continue? [Y/n] y
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion
-- xi2cps e0004000.ps7-i2c: timeout waiting on completion


...there is more but i cut it off

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 12 years ago

    Hi cuboard,

    Is this related to what is going on in these Xilinx forum posts?

    http://forums.xilinx.com/t5/Embedded-Linux/Microzed-i2c/m-p/395783

    http://forums.xilinx.com/t5/Embedded-Linux/Howto-compile-Zynq-Linux-with-I2C-driver/m-p/376793#M7209

    Looks like they might be using a devicetree entry like this rather than the one you are using:

    ps7-i2c@e0004000 {
                            compatible = "xlnx,ps7-i2c-1.00.a";
                            reg = <0xE0004000 0x1000>;
                            interrupts = <0 25 4>;
                            interrupt-parent = <0x2>;
                            bus-id = <0>;
    tttclock-names = "i2c9_aper";
    tttclocks = <0x3 39>;
                            input-clk = <111111111>;
                            i2c-clk = <100000>;t
                            #address-cells = <1>;
                            xlnx,i2c-clk-freq-hz = <0x69f6bcb>;
    ttt#size-cells = <0>;
                    };

    Have you tried an entry like this instead?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 12 years ago

    Hi cuboard,

    Is this related to what is going on in these Xilinx forum posts?

    http://forums.xilinx.com/t5/Embedded-Linux/Microzed-i2c/m-p/395783

    http://forums.xilinx.com/t5/Embedded-Linux/Howto-compile-Zynq-Linux-with-I2C-driver/m-p/376793#M7209

    Looks like they might be using a devicetree entry like this rather than the one you are using:

    ps7-i2c@e0004000 {
                            compatible = "xlnx,ps7-i2c-1.00.a";
                            reg = <0xE0004000 0x1000>;
                            interrupts = <0 25 4>;
                            interrupt-parent = <0x2>;
                            bus-id = <0>;
    tttclock-names = "i2c9_aper";
    tttclocks = <0x3 39>;
                            input-clk = <111111111>;
                            i2c-clk = <100000>;t
                            #address-cells = <1>;
                            xlnx,i2c-clk-freq-hz = <0x69f6bcb>;
    ttt#size-cells = <0>;
                    };

    Have you tried an entry like this instead?

    Regards,

    -Kevin