Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Access upper 16 MB of QSPI Flash
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Subscribers 363 subscribers
  • Views 3597 views
  • Users 0 members are here
Related

Access upper 16 MB of QSPI Flash

e14 Contributor
e14 Contributor over 13 years ago

The Zynq QSPI controller only supports 24-bit addressing (16 MB).  The Zedboard Hardware User Guide indicates the full 256 Mb capacity can be accessed via internal bank switching.

Does anybody know how to do this from Linux?  Is it possible to set up MTDs for both the lower and upper address ranges?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Thanks for the info Max.  Sounds like you guys are definitely working the issue.

    We have a Zynq Z-7045 design in the works.  The PL configuration file alone is over 12 MB, so there's no way that'll fit in 16 MB address space along the Linux image/ramdisk.  I'm trying to avoid using up the MIO pins for QSPI_1 just to gain the additional 16 MB for QSPI boot.

    The approach I'm trying to go with is boot into Linux using the lower 16 MB, and then switch to the upper 16 MB, read the configuration file and then configure the FPGA with xdevcfg.

    I'm hoping you guys and Xilinx can work out this issue so that Linux MTD is supported.  Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Thanks for the info Max.  Sounds like you guys are definitely working the issue.

    We have a Zynq Z-7045 design in the works.  The PL configuration file alone is over 12 MB, so there's no way that'll fit in 16 MB address space along the Linux image/ramdisk.  I'm trying to avoid using up the MIO pins for QSPI_1 just to gain the additional 16 MB for QSPI boot.

    The approach I'm trying to go with is boot into Linux using the lower 16 MB, and then switch to the upper 16 MB, read the configuration file and then configure the FPGA with xdevcfg.

    I'm hoping you guys and Xilinx can work out this issue so that Linux MTD is supported.  Thanks!