Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Access upper 16 MB of QSPI Flash
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Subscribers 363 subscribers
  • Views 3597 views
  • Users 0 members are here
Related

Access upper 16 MB of QSPI Flash

e14 Contributor
e14 Contributor over 13 years ago

The Zynq QSPI controller only supports 24-bit addressing (16 MB).  The Zedboard Hardware User Guide indicates the full 256 Mb capacity can be accessed via internal bank switching.

Does anybody know how to do this from Linux?  Is it possible to set up MTDs for both the lower and upper address ranges?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I think support fo 32 MB has been added lately.

    http://forums.xilinx.com/t5/Embedded-Linux/zc702-QSPI-Flash-Options-16-or-32-MB/m-p/345675#M6645

    http://forums.xilinx.com/t5/Embedded-Linux/Reboot-problem-when-QSPI-is-in-quad-I-O-mode/m-p/384851#M7317

    Still the user should be careful in designing an appropriate reset line to the flash device in order to reset it at its default state when rebooting.

    Best regards,
    Giulio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I think support fo 32 MB has been added lately.

    http://forums.xilinx.com/t5/Embedded-Linux/zc702-QSPI-Flash-Options-16-or-32-MB/m-p/345675#M6645

    http://forums.xilinx.com/t5/Embedded-Linux/Reboot-problem-when-QSPI-is-in-quad-I-O-mode/m-p/384851#M7317

    Still the user should be careful in designing an appropriate reset line to the flash device in order to reset it at its default state when rebooting.

    Best regards,
    Giulio