Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Petalinux Application with Graphic User Interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 2663 views
  • Users 0 members are here
Related

Petalinux Application with Graphic User Interface

e14 Contributor
e14 Contributor over 10 years ago

Hi everyone,
I have made a full working Linux (Petalinux) embedded project with partial reconfiguration technique on ZedBoard. I have written a bash script in which the user can choose when and which of reconfigurable modules have to be reconfigured. I would made the same thing but with a Graphic User Interface. How can I do that? Should I change the PL and add a VGA or HDMI ip's? Is there something already ready for petalinux, also with drivers? Can I do something just with the UART and bash(I was thinking about ncurses library or something like that..)? What kind of program to make a GUI?....I never did that before.

Any help will be useful! Thanks

Regards 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    What about if I did a "GUI" through the terminal? Is it possible to create something very simple? (I was thinking about ncurses library or something like that)..

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    What about if I did a "GUI" through the terminal? Is it possible to create something very simple? (I was thinking about ncurses library or something like that)..

    Thanks