Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development uart not functional in lab #5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 669 views
  • Users 0 members are here
Related

uart not functional in lab #5

e14 Contributor
e14 Contributor over 12 years ago

I am going through the LABS - associated with the ZedBoard videos, I'm stuck in Lab #5  (LED controller)- with the UART not functional.

The Hello World example works - so i know it is not the HW, that appears to be working correctly.

I can step through th code, the IO Address appears to be correct, I think - that perhaps the UART is not being initilized correctly.

Q: I see the BREAK at MAIN ... but how do I BREAK at _boot (the code that runs inIs there a way to stop/break at the reset vector and begin to debug I want to step through the UART initialization

Or is it something else that is initializing the uart?

Q: When the code reads from the UART status register, Im seeing the return value of e00002c  [the value of the status register I believe]


Any suggestions on where to go next?



  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I had inadvertently added UART 0 in one of the earlier labs and exported it, and that UART was set as the STDOUT uart.
    .
    UART 0 is not connected to the USB serial adapter, only UART 1
    .
    I figured it out by stepping through the code, and looking carefully at the base address of the UART passed to the BSP functions, the address was wrong...
    .
    -Duane.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I had inadvertently added UART 0 in one of the earlier labs and exported it, and that UART was set as the STDOUT uart.
    .
    UART 0 is not connected to the USB serial adapter, only UART 1
    .
    I figured it out by stepping through the code, and looking carefully at the base address of the UART passed to the BSP functions, the address was wrong...
    .
    -Duane.