Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development uart not functional in lab #5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 669 views
  • Users 0 members are here
Related

uart not functional in lab #5

e14 Contributor
e14 Contributor over 12 years ago

I am going through the LABS - associated with the ZedBoard videos, I'm stuck in Lab #5  (LED controller)- with the UART not functional.

The Hello World example works - so i know it is not the HW, that appears to be working correctly.

I can step through th code, the IO Address appears to be correct, I think - that perhaps the UART is not being initilized correctly.

Q: I see the BREAK at MAIN ... but how do I BREAK at _boot (the code that runs inIs there a way to stop/break at the reset vector and begin to debug I want to step through the UART initialization

Or is it something else that is initializing the uart?

Q: When the code reads from the UART status register, Im seeing the return value of e00002c  [the value of the status register I believe]


Any suggestions on where to go next?



  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    is the lab your are using from the Intro to Zynq video? If so the 'Hello World' serial output was directed to the SDK console while the serial output in lab5 should go to the USB-UART serial port. Make sure you set up the serial output as specified in the lab. You will need to have connected the ZedBoard USB-UART connection to a PC with a terminal program (like Tera Term or Putty for windows) and you need to have installed the driver for the Cypress USB-UART device on the PC. If you have done that and you still do not see the output you may need to enable the 'persist' mode on the Windows Cypress USB-UART device driver. Take a look at the answer here for instructions on how to do that if this is your issue:

    http://www.zedboard.org/content/problem-setting-sd

     

    Otherwise you might load the solution file for lab5 to insure that you did not make an error in the lab somewhere that is causing the issue.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    is the lab your are using from the Intro to Zynq video? If so the 'Hello World' serial output was directed to the SDK console while the serial output in lab5 should go to the USB-UART serial port. Make sure you set up the serial output as specified in the lab. You will need to have connected the ZedBoard USB-UART connection to a PC with a terminal program (like Tera Term or Putty for windows) and you need to have installed the driver for the Cypress USB-UART device on the PC. If you have done that and you still do not see the output you may need to enable the 'persist' mode on the Windows Cypress USB-UART device driver. Take a look at the answer here for instructions on how to do that if this is your issue:

    http://www.zedboard.org/content/problem-setting-sd

     

    Otherwise you might load the solution file for lab5 to insure that you did not make an error in the lab somewhere that is causing the issue.

     

    -Gary