Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development standalone OS  reference design problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 364 subscribers
  • Views 765 views
  • Users 0 members are here
Related

standalone OS  reference design problem

triacs
triacs over 9 years ago

I am trying to run the Zynq standalone OS embedded reference design on my MMP 7z045 eval board. In the Version 1 Aug 2015 instructions titled "Avnet Zynq Mini Module Plus Embedded Design", in section 7.3 Running the Memory Test, after I do the Run As > launch on Hardware GDB, I get SDK Application launcher window that says "Launch Failed, Binary not found. I followed all the instructions up to this point as written. Don't know what the problem is.  

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Triacs,

    Just to double check, you are using Vivado 2015.2 and SDK 2015.2 correct? And when you say your apply was already greyed out are you also indicating that your initialization file was already set to "\zynq_mmp_embedded_design\embedded_design.sdk\zynq_design_1_wrapper_hw_platform_1\ps7_init.tcl"

    Also for sanity check your boot configurations (SW5) is set to JTAG Boot correct "00000"?

    Also try using the System Debugger, do so by following these steps.

    1.Program the bit file into your FPGA(section 7.1) and make sure the Blue led is on. 

    2. Right click on your application then go Run as --> Run on hardware(System Debugger)

    let me know if your application runs or if you still have the same error.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Triacs,

    Just to double check, you are using Vivado 2015.2 and SDK 2015.2 correct? And when you say your apply was already greyed out are you also indicating that your initialization file was already set to "\zynq_mmp_embedded_design\embedded_design.sdk\zynq_design_1_wrapper_hw_platform_1\ps7_init.tcl"

    Also for sanity check your boot configurations (SW5) is set to JTAG Boot correct "00000"?

    Also try using the System Debugger, do so by following these steps.

    1.Program the bit file into your FPGA(section 7.1) and make sure the Blue led is on. 

    2. Right click on your application then go Run as --> Run on hardware(System Debugger)

    let me know if your application runs or if you still have the same error.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • triacs
    0 triacs over 9 years ago in reply to jafoste4

    I am running Vivado 2015.4. When I opened it it asked me if I wanted to upgrade the project, and I said yes. Yes, my init file already pointed to the correct path. (From previous running the project I assume). I'll try the System Debugger as you suggest.