Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picoZed boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 365 subscribers
  • Views 2724 views
  • Users 0 members are here
Related

picoZed boot

lguser
lguser over 8 years ago

Just recently I started working on the picoZed 7015 SOM board.  I have a few basic questions on boot. For prototyping and debugging, is it possible that we activate both SD (sdhci) controllers at the same time (one for SD and the other eMMC) ?  (In production we will use eMMC only.)  

While awaiting hardware to generate the HDF file, is there a sample HDF file for this board so I can build the FSBL?

In the meantime, I loaded Xilinx U-boot (2017) on the picoZed.  Expectedly, the boot failed with no output. This U-boot image uses SPL as the FSBL and it was built for the picoZed via the following commands (without the proper ps7_init_gpl.c from HDF) :

  make zynq_picozed_defconfig; make

I had a Xilinx ZC702 board. So I loaded the ZC702 U-boot (built with zynq_zc702_defconfig) on this picoZed board. Surprisingly it went further and it was searching for the U-boot proper image (u-boot.img), 

  spl: error reading image u-boot.img

Am I missing anything?  Will zynq_picozed_defconfig work if I provide the proper ps7_init_gpl.c file?  

If SPL is not used in U-boot, is there anything we need to supply U-boot for picoZed?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 8 years ago

    Hi lguser,

    I believe that is should be possible to enable both SD card and eMMC simultaneously since they are on separate PS SDIO interfaces.

    I am not familiar with the use of SPL on any of our boards since most of our Linux development is driven with PetaLinux. We do have PetaLinux BSPs available for each of the PicoZed SOM variants (z7010, z7015, z7020, and z7030) available for download from the PicoZed V2 Carrier Reference Design/Tutorial page:

    http://www.picozed.org/support/design/13076/106

    The PetaLinux BSPs should contain an HDF for the pre-built Vivado hardware platform along with an archived version of the Vivado project that the HDF is generated from.

    Perhaps these PetaLinux BSP would serve as a good starting point to answer some of your questions on how U-Boot can be built and later customized to fit your end application needs?

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 8 years ago

    Hi lguser,

    I believe that is should be possible to enable both SD card and eMMC simultaneously since they are on separate PS SDIO interfaces.

    I am not familiar with the use of SPL on any of our boards since most of our Linux development is driven with PetaLinux. We do have PetaLinux BSPs available for each of the PicoZed SOM variants (z7010, z7015, z7020, and z7030) available for download from the PicoZed V2 Carrier Reference Design/Tutorial page:

    http://www.picozed.org/support/design/13076/106

    The PetaLinux BSPs should contain an HDF for the pre-built Vivado hardware platform along with an archived version of the Vivado project that the HDF is generated from.

    Perhaps these PetaLinux BSP would serve as a good starting point to answer some of your questions on how U-Boot can be built and later customized to fit your end application needs?

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • bhfletcher
    0 bhfletcher over 8 years ago in reply to zedhed

    You definitely can use both SD Card and eMMC simultaneously on PicoZed. They are on separate PS SDIO interfaces as zedhed states. However, remember that the SD Card can be used for either primary or secondary boot on Zynq-7000, while the eMMC can be used for secondary boot only. You will need to use the QSPI for primary boot with eMMC for secondary boot.

    Bryan