Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picoZed boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 365 subscribers
  • Views 2723 views
  • Users 0 members are here
Related

picoZed boot

lguser
lguser over 8 years ago

Just recently I started working on the picoZed 7015 SOM board.  I have a few basic questions on boot. For prototyping and debugging, is it possible that we activate both SD (sdhci) controllers at the same time (one for SD and the other eMMC) ?  (In production we will use eMMC only.)  

While awaiting hardware to generate the HDF file, is there a sample HDF file for this board so I can build the FSBL?

In the meantime, I loaded Xilinx U-boot (2017) on the picoZed.  Expectedly, the boot failed with no output. This U-boot image uses SPL as the FSBL and it was built for the picoZed via the following commands (without the proper ps7_init_gpl.c from HDF) :

  make zynq_picozed_defconfig; make

I had a Xilinx ZC702 board. So I loaded the ZC702 U-boot (built with zynq_zc702_defconfig) on this picoZed board. Surprisingly it went further and it was searching for the U-boot proper image (u-boot.img), 

  spl: error reading image u-boot.img

Am I missing anything?  Will zynq_picozed_defconfig work if I provide the proper ps7_init_gpl.c file?  

If SPL is not used in U-boot, is there anything we need to supply U-boot for picoZed?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 8 years ago

    Hi lguser,

    I believe that is should be possible to enable both SD card and eMMC simultaneously since they are on separate PS SDIO interfaces.

    I am not familiar with the use of SPL on any of our boards since most of our Linux development is driven with PetaLinux. We do have PetaLinux BSPs available for each of the PicoZed SOM variants (z7010, z7015, z7020, and z7030) available for download from the PicoZed V2 Carrier Reference Design/Tutorial page:

    http://www.picozed.org/support/design/13076/106

    The PetaLinux BSPs should contain an HDF for the pre-built Vivado hardware platform along with an archived version of the Vivado project that the HDF is generated from.

    Perhaps these PetaLinux BSP would serve as a good starting point to answer some of your questions on how U-Boot can be built and later customized to fit your end application needs?

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    Kevin, thanks a lot for the information.  

    I have Vivado 2017.4 downloaded early this year (2018).  I just downloaded 01_MZPZ_Zynq_Intro_2016_4_01.pdf from the link you provided. I am following the instructions on page 6.  Figure 5 is showing many different picozed boards, but my Vivado only shows 'ZedBoard Zynq Evaluation and Development Kit'.  Do I have to download Vivado 2016.4?  Is there a way to upgrade my 2017.4 to the lastest version?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Did you install the Board Definition files for PicoZed? Please go to this link http://zedboard.org/support/documentation/13076

    and install PicoZed Board Definition Install for Vivado 2015.3 through 2017.4

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    Kevin, I extracted the pciozed directories/files from www.picozed.org and copied them under Vivado/2017.4/data/board/board_files directory.  However, when I tried to create a new project, only 'ZedBoard Zynq Evaluation and Development Kit' shows up on the "Default Part" screen .  I didn't see the picoZed boards displayed.  Did I miss anything?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    Josh, I didn't see your post earlier.  Thanks for the info.  Yes.  I extracted the files from http://www.picozed.org/support/documentation/13076 and placed them under the data/board/board_files/ directory.  Do I need to refresh Vivado?  Did I miss any step?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    After you add them, you will need to close and reopen Vivado.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 8 years ago in reply to zedhed

    You definitely can use both SD Card and eMMC simultaneously on PicoZed. They are on separate PS SDIO interfaces as zedhed states. However, remember that the SD Card can be used for either primary or secondary boot on Zynq-7000, while the eMMC can be used for secondary boot only. You will need to use the QSPI for primary boot with eMMC for secondary boot.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    Josh, thanks for the info and I was able to generate the default HDF file and the FSBL based on the instructions in tuturials 01 and 04.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    Hi Byran, thanks for the info.  Is the sdhci controller for the eMMC by default configured and enabled by the FSBL?  By the way, is the eMMC/JX2 MIO multiplexer automatically configured to select eMMC?  Do we need to modify the device-tree (u-boot/Linux) to turn it on?    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lguser
    0 lguser over 8 years ago

    How do I generate the device tree file from either Vivado or Xilinx SDK?  This device tree is intended for booting Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>