Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picoZed boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 365 subscribers
  • Views 2724 views
  • Users 0 members are here
Related

picoZed boot

lguser
lguser over 8 years ago

Just recently I started working on the picoZed 7015 SOM board.  I have a few basic questions on boot. For prototyping and debugging, is it possible that we activate both SD (sdhci) controllers at the same time (one for SD and the other eMMC) ?  (In production we will use eMMC only.)  

While awaiting hardware to generate the HDF file, is there a sample HDF file for this board so I can build the FSBL?

In the meantime, I loaded Xilinx U-boot (2017) on the picoZed.  Expectedly, the boot failed with no output. This U-boot image uses SPL as the FSBL and it was built for the picoZed via the following commands (without the proper ps7_init_gpl.c from HDF) :

  make zynq_picozed_defconfig; make

I had a Xilinx ZC702 board. So I loaded the ZC702 U-boot (built with zynq_zc702_defconfig) on this picoZed board. Surprisingly it went further and it was searching for the U-boot proper image (u-boot.img), 

  spl: error reading image u-boot.img

Am I missing anything?  Will zynq_picozed_defconfig work if I provide the proper ps7_init_gpl.c file?  

If SPL is not used in U-boot, is there anything we need to supply U-boot for picoZed?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Did you install the Board Definition files for PicoZed? Please go to this link http://zedboard.org/support/documentation/13076

    and install PicoZed Board Definition Install for Vivado 2015.3 through 2017.4

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hi,

    Did you install the Board Definition files for PicoZed? Please go to this link http://zedboard.org/support/documentation/13076

    and install PicoZed Board Definition Install for Vivado 2015.3 through 2017.4

    Thanks,

    Josh