Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picoZed boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 365 subscribers
  • Views 2724 views
  • Users 0 members are here
Related

picoZed boot

lguser
lguser over 8 years ago

Just recently I started working on the picoZed 7015 SOM board.  I have a few basic questions on boot. For prototyping and debugging, is it possible that we activate both SD (sdhci) controllers at the same time (one for SD and the other eMMC) ?  (In production we will use eMMC only.)  

While awaiting hardware to generate the HDF file, is there a sample HDF file for this board so I can build the FSBL?

In the meantime, I loaded Xilinx U-boot (2017) on the picoZed.  Expectedly, the boot failed with no output. This U-boot image uses SPL as the FSBL and it was built for the picoZed via the following commands (without the proper ps7_init_gpl.c from HDF) :

  make zynq_picozed_defconfig; make

I had a Xilinx ZC702 board. So I loaded the ZC702 U-boot (built with zynq_zc702_defconfig) on this picoZed board. Surprisingly it went further and it was searching for the U-boot proper image (u-boot.img), 

  spl: error reading image u-boot.img

Am I missing anything?  Will zynq_picozed_defconfig work if I provide the proper ps7_init_gpl.c file?  

If SPL is not used in U-boot, is there anything we need to supply U-boot for picoZed?

  • Sign in to reply
  • Cancel
Parents
  • lguser
    0 lguser over 8 years ago

    How do I generate the device tree file from either Vivado or Xilinx SDK?  This device tree is intended for booting Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • lguser
    0 lguser over 8 years ago

    How do I generate the device tree file from either Vivado or Xilinx SDK?  This device tree is intended for booting Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • drozwood90
    0 drozwood90 over 8 years ago in reply to lguser

    Please start new threads for things like this.
    You will want to go through the most recent PetaLinux SpeedWay.
    Integrating Sensors on MiniZed with PetaLinux (2017.1 and 2017.4)
    http://zedboard.org/support/trainings-and-videos