Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Execution time measurement
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 2519 views
  • Users 0 members are here
Related

Execution time measurement

e14 Contributor
e14 Contributor over 12 years ago

Hello,
I am using zedboard for my project and I want to measure my algorithm process time. The problem is that I can not use the clock() or gettimeofday() function, it says "undefined reference to _gettimeofday" or " undefined reference to _time", but in fact, I have already included the <sys/time.h> and <time.h>. I really need this problem to be fixed or any idea to measure the execution time.

P.S. My programmm is based on C and neon intrinsics, and the The Project is running on standalone. 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    It's not that you don't have the right header - the link stage is failing because you don't have the libraries.

    I just reproduced your problem - my project is on "bare metal" at the moment too.  Calling the clock functions in "time.h" seems to cause a linker error:

    [code]
    Building target: CppPlay.elf
    Invoking: ARM g++ linker
    arm-xilinx-eabi-g++ -Wl,-T -Wl,../src/lscript.ld -L../../microZedAndIOCC_bsp_0/ps7_cortexa9_0/lib -o "CppPlay.elf"  ./src/dpiocc.o ./src/main.o ./src/platform.o   -Wl,--start-group,-lxil,-lgcc,-lc,-lstdc++,--end-group -Wl,--start-group,-lxilffs,-lxil,-lgcc,-lc,--end-group -Wl,--start-group,-lxilisf,-lxil,-lgcc,-lc,--end-group -Wl,--start-group,-lxil,-llwip4,-lgcc,-lc,--end-group
    /home/dean/Xilinx/SDK/2014.1/gnu/arm/lin/bin/../lib/gcc/arm-xilinx-eabi/4.8.1/../../../../arm-xilinx-eabi/lib/libc.a(lib_a-timesr.o): In function `_times_r':
    timesr.c:(.text+0x4): undefined reference to `_times'
    collect2: error: ld returned 1 exit status
    [/code]

    Perhaps the standard library is missing some functions, or we are missing a linker parameter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    This stack overflow article seems to describe the problem.
    http://stackoverflow.com/questions/15030123/how-does-the-clock-function-in-ctime-access-the-system-clock

    It might just be easier to use one of the PS timers; Adam Taylor has a nice intro:
    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Implementing-the-Zynq-SoC-s-Private-Timer-Adam-Taylor-s-MicroZed/ba-p/402203

    This gave me an excuse to play with the timer stuff, the attached is a working 100 microsecond timer with a stub function that seems to satisfy _that one particular_ missing library function (ie: ymmv); two files 'substitute_times.h' and 'substitute_times.cpp'

    **/// snip ///**

    /*
    * substitute_times.h
    *
    *  simple interrupt driven timer to stand-in for standard lib
    *  function 'times'
    */

    #ifndef SUBSTITUTE_TIMES_H_
    #define SUBSTITUTE_TIMES_H_

    #include <xscugic.h>

    ///@note the arm-xilinx-eabi library function '_times' itself already declared; we won't do it again

    /** Installs a timer interrupt handler and initialize the system timer to generate a timer interrupt every 100 microseconds.
    * The interrupt routine maintains a software divider to generate CLOCKS_PER_SEC frequency.
    * and install a handler to process the interrupt and increment a counter.
    * @note call from your interrupt configuration routine, before you globally enable interrupts.
    * @note enables timer interrupt and also GIC interrupt for timer.
    * @param pInterruptControllertreference to interrupt controller
    */
    void init_substitute_times(XScuGic *pInterruptController);

    /** stop the interrupts, kill the timer */
    void kill_substitute_times();

    /** elapsed microseconds since boot */
    uint64_t getMicroseconds();

    /** elapsed CLOCKS_PER_SEC since boot */
    clock_t getClocks();

    #endif /* SUBSTITUTE_TIMES_H_ */

    **/// snip ///**

    /*
    * substitute_times.cpp
    */

    #include <stdint.h>
    #include <ctime>
    #include <sys/times.h>

    #include <xil_types.h>
    #include <xparameters.h>
    #include <xscutimer.h>
    #include <xscugic.h>

    /**tTimer interrupt period in microseconds.
    *
    * from "xparameters.h" we know that
    * XPAR_PS7_CORTEXA9_0_CPU_CLK_FREQ_HZ is system clock (~667MHz on my microZed)
    *
    * from the Zynq-700 SoC reference we know that:
    * tt8.2.1 Clocking
    *ttAll private timers and watchdog timers are always clocked at 1/2 of the CPU frequency (CPU_3x2x).
    *
    * from "time.h" we know CLOCKS_PER_SEC = 100.
    *
    * so for example we can use 3333333 as a divisor for 100.00001305 Hz
    *
    * From <http://forums.xilinx.com/t5/Xcell-Daily-Blog/Implementing-the-Zynq-SoC-s-Private-Timer-Adam-Taylor-s-MicroZed/ba-p/402203>
    * twe steal code liberally...
    *
    */
    const uint32_t timer_period_microseconds = 100;

    const uint32_t timer_freq = 1000000/timer_period_microseconds;

    /**tTimer divisor to give us 'timer_period_microseconds' intervals
    */
    const uint32_t divisor_for_timer = (XPAR_PS7_CORTEXA9_0_CPU_CLK_FREQ_HZ/2) / timer_freq;

    const uint32_t timer_periods_per_CLOCK = timer_freq/CLOCKS_PER_SEC;


    /// incremented at CLOCKS_PER_SEC by timer interrupt
    volatile clock_t clock_value = 0;


    /// will contain ref to ARM 'private' timer
    static XScuTimer substitute_tick_timer;

    /// incremented every 'timer_period_microseconds' by timer interrupt; not necessarily incremented by 1 !!
    volatile uint64_t microsecond_counter = 0;

    // incremented each timer interrupt, when it equals timer_periods_per_CLOCK then 'clock_value' is incremented
    volatile uint64_t CLOCK_counter = 0;

    /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

    extern "C"
    {
    t/** substitute for missing arm-xilinx-eabi library '_times' symbol.
    t * @note the '_times' function itself already declared; we won't do it again
    t */
    tclock_t _times(tms * ptms)
    t{
    ttif (ptms)
    tt{
    ttt// fill in struct in vaguely appropriate fashion
    tttptms->tms_utime = 0;  /* user time */
    tttptms->tms_stime = clock_value;  /* system time */
    tttptms->tms_cutime = 0; /* user time of children */
    tttptms->tms_cstime = 0; /* system time of children */
    tt}
    ttreturn clock_value;
    t}
    }
    /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

    uint64_t getMicroseconds() { return microsecond_counter; }
    clock_t getClocks() { return clock_value; }

    /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

    /** timer interrupt handler
    * @param CallBackRefta reference to our XScuTimer
    */
    static void handler_substitue_times(void *CallBackRef)
    {
    tXScuTimer *pTimer = (XScuTimer *) CallBackRef;t// ideally, equal to 'substitute_tick_timer'

    tmicrosecond_counter += timer_period_microseconds;

    tCLOCK_counter += 1;
    tif (CLOCK_counter == timer_periods_per_CLOCK)
    t{
    ttclock_value += 1;
    ttCLOCK_counter = 0;
    t}

    tXScuTimer_ClearInterruptStatus(pTimer);
    }

    /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

    void init_substitute_times(XScuGic *pInterruptController)
    {
        //timer initialization

    tXScuTimer_Config* pTimerConfig = XScuTimer_LookupConfig(XPAR_XSCUTIMER_0_DEVICE_ID);

    tif (pTimerConfig)
    t{
    ttXScuTimer_CfgInitialize(&substitute_tick_timer, pTimerConfig, pTimerConfig->BaseAddr);

    ttXScuTimer_SelfTest(&substitute_tick_timer); // hmmm

    tt//load the timer

    ttXScuTimer_LoadTimer(&substitute_tick_timer, divisor_for_timer);
    t tXScuTimer_EnableAutoReload(&substitute_tick_timer);

    t t//set up the interrupts
    ttXScuGic_Connect(pInterruptController, XPAR_SCUTIMER_INTR, (Xil_ExceptionHandler)handler_substitue_times, (void *)&substitute_tick_timer);

    tt//enable the interrupt for the Timer at GIC
    ttXScuGic_Enable(pInterruptController, XPAR_SCUTIMER_INTR);
    tt//enable interrupt on the timer
    ttXScuTimer_EnableInterrupt(&substitute_tick_timer);

    t t//start timer
    t tXScuTimer_Start(&substitute_tick_timer);
    t}
    telse
    t{
    tt// whoops, no timer? bad ID?
    t}
    }

    void kill_substitute_times()
    {
    t//disable interrupt on the timer
    tXScuTimer_DisableInterrupt(&substitute_tick_timer);
    tXScuTimer_Stop(&substitute_tick_timer);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks so much for the reply.
    I want to try your header file, but the funny thing is that when I include xscugic.h header, it say "no such file or directory". And also the xscutimer.h and xil_types.h . But the fact is that I can find these files in the Myproject_bsp folder.
    Do you know the reason?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    First, I'm pretty much in the dark as to how (even where) the make files for the SDK projects are being stored and manipulated...

    But I'll take a guess about your problem.

    So in the SDK your application project (in the SDK project explorer pane) has a little Folder icon with "C" on it.

    Right click on that and down the bottom is "Change Referenced BSP" - is that referencing the correct BSP?

    Also, again, right clicking on the application project, "Build Settings" brings up a dialog box with a "Tool Settings" tab.  In that tab click on "ARM g++ compiler" and you should see:
          Command: arm-xilinx-eabi-g++
      All Options: -Wall -O0 -g3 -c -fmessage-length=0 -I../../microZedAndIOCC_bsp_0/ps7_cortexa9_0/include

    that -I option is the include path for GCC - which is pointing to my BSP.

    If either of those things doesn't look right, maybe you should try exporting your hardware again from Vivado and rebuilding your BSP?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for the fast reply!

    The solution is exactly the same as my settings. like:
    1. the referenced BSP is test_neon_alone_bsp.
    2. And also, I think the Build settings is almost the same, because I am using "Xilinx ARM GNU Toolchain" and builder is "GNU make", so I see:
    Command: arm-xilinx-eabi-gcc
    All Options: -Wall -O0 -g3 -c -fmessage-length=0 -I../../test_neon_alone_bsp/ps7_cortexa9_0/include

    In which test_neon_alone is my project name. 

    So I really don't have any clue about this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor


    **** Build of configuration Debug for project test_neon_alone ****

    make all
    Building file: ../src/helloworld.c
    Invoking: ARM gcc compiler
    arm-xilinx-eabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"src/helloworld.d" -MT"src/helloworld.d" -o"src/helloworld.o" "../src/helloworld.c"
    In file included from ../src/helloworld.c:41:0:
    ../src/substitut_timer.h:17:21: fatal error: xscugic.h: No such file or directory
    compilation terminated.
    make: *** [src/helloworld.o] Fehler 1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    compare:
    All Options: -Wall -O0 -g3 -c -fmessage-length=0 -I../../test_neon_alone_bsp/ps7_cortexa9_0/include

    and

    arm-xilinx-eabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"src/helloworld.d" -MT"src/helloworld.d" -o"src/helloworld.o" "../src/helloworld.c"

    I don't see the -I in the compiler invocation.

    Perhaps you could try this:
    Right click you your "helloworld,c" in the project and view the properties.
    In C/C++ Build | Settings - ARM g++ compiler

    Do you see the include path in your "All options" text??

    Maybe try the "Restore Defaults" button?