Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Execution time measurement
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 2521 views
  • Users 0 members are here
Related

Execution time measurement

e14 Contributor
e14 Contributor over 12 years ago

Hello,
I am using zedboard for my project and I want to measure my algorithm process time. The problem is that I can not use the clock() or gettimeofday() function, it says "undefined reference to _gettimeofday" or " undefined reference to _time", but in fact, I have already included the <sys/time.h> and <time.h>. I really need this problem to be fixed or any idea to measure the execution time.

P.S. My programmm is based on C and neon intrinsics, and the The Project is running on standalone. 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    First, I'm pretty much in the dark as to how (even where) the make files for the SDK projects are being stored and manipulated...

    But I'll take a guess about your problem.

    So in the SDK your application project (in the SDK project explorer pane) has a little Folder icon with "C" on it.

    Right click on that and down the bottom is "Change Referenced BSP" - is that referencing the correct BSP?

    Also, again, right clicking on the application project, "Build Settings" brings up a dialog box with a "Tool Settings" tab.  In that tab click on "ARM g++ compiler" and you should see:
          Command: arm-xilinx-eabi-g++
      All Options: -Wall -O0 -g3 -c -fmessage-length=0 -I../../microZedAndIOCC_bsp_0/ps7_cortexa9_0/include

    that -I option is the include path for GCC - which is pointing to my BSP.

    If either of those things doesn't look right, maybe you should try exporting your hardware again from Vivado and rebuilding your BSP?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor


    **** Build of configuration Debug for project test_neon_alone ****

    make all
    Building file: ../src/helloworld.c
    Invoking: ARM gcc compiler
    arm-xilinx-eabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"src/helloworld.d" -MT"src/helloworld.d" -o"src/helloworld.o" "../src/helloworld.c"
    In file included from ../src/helloworld.c:41:0:
    ../src/substitut_timer.h:17:21: fatal error: xscugic.h: No such file or directory
    compilation terminated.
    make: *** [src/helloworld.o] Fehler 1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor


    **** Build of configuration Debug for project test_neon_alone ****

    make all
    Building file: ../src/helloworld.c
    Invoking: ARM gcc compiler
    arm-xilinx-eabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"src/helloworld.d" -MT"src/helloworld.d" -o"src/helloworld.o" "../src/helloworld.c"
    In file included from ../src/helloworld.c:41:0:
    ../src/substitut_timer.h:17:21: fatal error: xscugic.h: No such file or directory
    compilation terminated.
    make: *** [src/helloworld.o] Fehler 1