Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PetaLinux 2016.3 Compressed BSP, z7010
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 648 views
  • Users 0 members are here
Related

PetaLinux 2016.3 Compressed BSP, z7010

e14 Contributor
e14 Contributor over 9 years ago

Hi

I'm searching for the:

PetaLinux 2016.3 Compressed BSP, z7010.

I'm using Linux 16.04 LTS Linux with Vivado 2016.3 and Petalinux 2016.3 and i'm working on a microzed board 7z010 rev F. If there is no such BSP is one of the older ones compatible with the new Petalinux version?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Zwygd,

    As of right now we only have up to Petalinux 2016.2 BSP released for MicroZed, and we are only offering support for the even releases of Petalinux meaning 2016.4, 2017.2, 2017.4 releases. This means we have no plans to create a 2016.3 Petalinux BSP for the MicroZed.

    It is also suggested that you do not Mix and Match older Petalinux BSPs with other Petalinux releases. 

    If you want to use Petalinux 2016.3, then you will need to create your own MicroZed 2016.3 BSP. I am going to refer you to this post which goes over the steps that are needed to generate your own BSP. http://zedboard.org/content/petalinux-20152-bsp-microzed

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Zwygd,

    As of right now we only have up to Petalinux 2016.2 BSP released for MicroZed, and we are only offering support for the even releases of Petalinux meaning 2016.4, 2017.2, 2017.4 releases. This means we have no plans to create a 2016.3 Petalinux BSP for the MicroZed.

    It is also suggested that you do not Mix and Match older Petalinux BSPs with other Petalinux releases. 

    If you want to use Petalinux 2016.3, then you will need to create your own MicroZed 2016.3 BSP. I am going to refer you to this post which goes over the steps that are needed to generate your own BSP. http://zedboard.org/content/petalinux-20152-bsp-microzed

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • 100zaheer
    0 100zaheer over 9 years ago in reply to jafoste4

    Hey Josh,

    Where can i find Petalinux 2016.4, 2017.2, 2017.4 BSP for MicroZed board?

    Zaheer R M