Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PicoZed: Frequent i2c-cadence driver timeouts when using real-time kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 3493 views
  • Users 0 members are here
Related

PicoZed: Frequent i2c-cadence driver timeouts when using real-time kernel

100sky
100sky over 8 years ago

Hello,

i have encounter several I2C timeout issues on an AVNET picoZed Z7020 board when accessing an I2C device using a real-time kernel when booting the device.

I.e. at each 3-5 reboots an I2C timeout occurs and the I2C device must be restarted in order to get the I2C working again. However, restarting the I2C device is not feasible for us.

The problem happens also on non-real-time kernels but much less frequent, i.e. roughly at 1 of 100 reboots the error occurs.

The error which is reported is following:

cdns-i2c e0004000.ps7-i2c: timeout waiting on completion

During the Linux boot (4.14.24), a program on the Linux system is started which transceives quite a large amount of data to the I2C device (but only max. 261 bytes at once over I2C).

I do not think that this is an HW issue since it works in a few times. However, I have tried to change the pullups for the I2C device from 1k to 2k without any success. (Next will be to increase the pullups to 4k.)

What I have figured out is that when the program (which transceives the I2C data during boot) on the Linux system is "interrupted" by another program (which has nothing to do with an I2C access at all, e.g. apache2) the timeout occurs. 

The interruption takes place when waiting within the I2C cadence driver' cdns_i2c_process_msg() function I think which results that cdns_i2c_mrecv does not return any data within the given adap->timeout (1000ms / 250 jiffies).

[...]
cdns_i2c_mrecv(id);
[...]
/* Wait for the signal of completion */
time_left = wait_for_completion_timeout(&id->xfer_done, adap->timeout);
[...]
 
Further investigation showed me the the following comment within the i2c-cadence driver:
/*
 * Cadence I2C controller has a bug wherein it generates
 * invalid read transaction after HW timeout in master receiver mode.
 * HW timeout is not used by this driver and the interrupt is disabled.
 * But the feature itself cannot be disabled. Hence maximum value
 * is written to this register to reduce the chances of error.
 */

Does anyone has some ideas what this issue could be and maybe how this can be solved? Does this comment might possible happen to our real-time-kernel very often?
 
Thank you & kind regards,
-
  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Sky,

    Are you using the Zynqs hardened I2C PC controller? Or are you using an axi I2C controller. We have seen many issues with the PS I2C controller and encourage our customers to use the PL AXI I2C controller for their application.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100sky
    0 100sky over 8 years ago

    Hi!

     

    I am not sure what the PL AXI I2C controller is, but I am quite sure that I use the PS I2C controller. I currently never heard about the PL AXI I2C controller. How can I enable it or use it?

    Thanks in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    When you are generating your Vivado block design you instantiate it in the PL.

    Please refer to Tutorial 08

    http://zedboard.org/support/design/18891/146

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100sky
    0 100sky over 8 years ago

    It seems that there are bugs in the i2c-cadence controller on ZYNQ 7000 platform and the driver which are not fixed yet (and also no fix planned in future). See posts here: https://forums.xilinx.com/t5/Embedded-Linux/Cadence-I2C-driver-bug/td-p/854621 for workarounds.

    I.e.: following bugs affect me:

    •   https://www.xilinx.com/support/answers/61665.html
    •   https://www.xilinx.com/support/answers/61664.html

    I have implemented these workarounds within the i2c-cadence driver and it seems that it works now. 

    PL changes are not possible for us! Therefore this is no solution yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer