Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PicoZed: Frequent i2c-cadence driver timeouts when using real-time kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 3494 views
  • Users 0 members are here
Related

PicoZed: Frequent i2c-cadence driver timeouts when using real-time kernel

100sky
100sky over 8 years ago

Hello,

i have encounter several I2C timeout issues on an AVNET picoZed Z7020 board when accessing an I2C device using a real-time kernel when booting the device.

I.e. at each 3-5 reboots an I2C timeout occurs and the I2C device must be restarted in order to get the I2C working again. However, restarting the I2C device is not feasible for us.

The problem happens also on non-real-time kernels but much less frequent, i.e. roughly at 1 of 100 reboots the error occurs.

The error which is reported is following:

cdns-i2c e0004000.ps7-i2c: timeout waiting on completion

During the Linux boot (4.14.24), a program on the Linux system is started which transceives quite a large amount of data to the I2C device (but only max. 261 bytes at once over I2C).

I do not think that this is an HW issue since it works in a few times. However, I have tried to change the pullups for the I2C device from 1k to 2k without any success. (Next will be to increase the pullups to 4k.)

What I have figured out is that when the program (which transceives the I2C data during boot) on the Linux system is "interrupted" by another program (which has nothing to do with an I2C access at all, e.g. apache2) the timeout occurs. 

The interruption takes place when waiting within the I2C cadence driver' cdns_i2c_process_msg() function I think which results that cdns_i2c_mrecv does not return any data within the given adap->timeout (1000ms / 250 jiffies).

[...]
cdns_i2c_mrecv(id);
[...]
/* Wait for the signal of completion */
time_left = wait_for_completion_timeout(&id->xfer_done, adap->timeout);
[...]
 
Further investigation showed me the the following comment within the i2c-cadence driver:
/*
 * Cadence I2C controller has a bug wherein it generates
 * invalid read transaction after HW timeout in master receiver mode.
 * HW timeout is not used by this driver and the interrupt is disabled.
 * But the feature itself cannot be disabled. Hence maximum value
 * is written to this register to reduce the chances of error.
 */

Does anyone has some ideas what this issue could be and maybe how this can be solved? Does this comment might possible happen to our real-time-kernel very often?
 
Thank you & kind regards,
-
  • Sign in to reply
  • Cancel
Parents
  • 100sky
    0 100sky over 8 years ago

    Hi!

     

    I am not sure what the PL AXI I2C controller is, but I am quite sure that I use the PS I2C controller. I currently never heard about the PL AXI I2C controller. How can I enable it or use it?

    Thanks in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100sky
    0 100sky over 8 years ago

    Hi!

     

    I am not sure what the PL AXI I2C controller is, but I am quite sure that I use the PS I2C controller. I currently never heard about the PL AXI I2C controller. How can I enable it or use it?

    Thanks in advance!