Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development [Solved] linaro-ubuntu:how to make u-boot use mmcblk0p2as rootfs,but not ramdisk?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 800 views
  • Users 0 members are here
Related

[Solved] linaro-ubuntu:how to make u-boot use mmcblk0p2as rootfs,but not ramdisk?

e14 Contributor
e14 Contributor over 13 years ago

I have doing linaro-ubuntu-desktop for several days,
last week I was doing as a pdf says(from http://www.zedboard.org/design) ubuntu_desktop,but failed,the error message is
:
/***********************code

Error: unrecognized/unsupported machine ID (r1 = 0x1fb71dd0).                  
                       
Available machine support:                                                                                                
ID (hex)        NAME                                                          
00000d32        Xilinx Zynq Platform

*****************code*/

I think it's maybe because the solution's out of date.

yesterday and today, I'm doing as analog adv7511 demo.

its website is http://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq

the u-boot.elf is built as   http://www.wiki.xilinx.com/U-boot
and the xilinx u-boot is configured to use ramdisk rootfs.
so the boot.bin requires uImage devicetree.dtb and uramdisk.tar.gz

I want to use mmcblk0p2 (the SDcard ext4 partition)
Here's my problem:

1.if there's no uramdisk in the fat32 partition,the boot.bin will cancel. and then the linux won't continue to boot

2.if I do copy a uramdisk.tar.gz into the fat32 partition, it will boot OK,but won't use mmcblkp2 as rootfs.  so it's just a simple linux, without linaro ubuntu.

what should I do to make the linaro-ubuntu-desktop boot?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I used to be stuck on this problem.

    The current Xilinx u-boot and kernel expect to boot with bootm, not go.

    bootm has three arguments: <kernel-addr> <ramdisk-addr> <devicetree-addr>.

    To boot to the rootfs on the SD card, you want to run:
    "bootm kernel - devicetree"
    which tells bootm and the kernel there IS no ramdisk.

    You can override u-boot autoboot and type this command yourself, or you can modify the u-boot source code to change what commands it issues to autoboot.

    Also your devicetree should have a bootargs string which defines rootfs as /dev/mmcblk0p2.

    Please see http://fpgacpu.wordpress.com/2013/05/24/yet-another-guide-to-running-linaro-ubuntu-desktop-on-xilinx-zynq-on-the-zedboard/ for a more thorough explanation and tutorial.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I used to be stuck on this problem.

    The current Xilinx u-boot and kernel expect to boot with bootm, not go.

    bootm has three arguments: <kernel-addr> <ramdisk-addr> <devicetree-addr>.

    To boot to the rootfs on the SD card, you want to run:
    "bootm kernel - devicetree"
    which tells bootm and the kernel there IS no ramdisk.

    You can override u-boot autoboot and type this command yourself, or you can modify the u-boot source code to change what commands it issues to autoboot.

    Also your devicetree should have a bootargs string which defines rootfs as /dev/mmcblk0p2.

    Please see http://fpgacpu.wordpress.com/2013/05/24/yet-another-guide-to-running-linaro-ubuntu-desktop-on-xilinx-zynq-on-the-zedboard/ for a more thorough explanation and tutorial.