Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Accelerating openCV with zynq on Zedboard (Xilinx appnote 1167)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 930 views
  • Users 0 members are here
Related

Accelerating openCV with zynq on Zedboard (Xilinx appnote 1167)

e14 Contributor
e14 Contributor over 13 years ago

Hi,
I am trying to run newly realeased xapp1167(http://www.xilinx.com/support/documentation/application_notes/xapp1167.pdf) for accelerating openCV with zynq on Zedboard. That app is originally for zc702 board. At first I tried to run this application as it is explained but did not work on Zedboard (expected).

In  order to run this on zed board, I created a new boot.bin file (by make boot as in app note) using the FSBL  and U-Boot binary for Zedboard from xilinx wiki release (http://www.wiki.xilinx.com/Zynq+14.5+-+2013.1+Release). Also replaced the devicetree.dtb file in the sd_image  with the one for ZedBoard from above release. Now I am able to boot the processors. but when i try to run the application i get following error
zynq> ./run.sh
Error : cann't open framebuffer device /dev/fb0

The application needs to interact with hdmi port but I suspect it is somehow not detected. Can anyone suggest me what needs to be done in order to get the hdmi port working or simply get rid of this error.

thanks
umair

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    We had a lot issues setting up and run  XAPP1167 as well.   However, we did get it working by exporting the Vivado HLS code as a ISE compatible IP, than start from XAPP890 and replace the Sobel filter IP with Fast IP (all connection stays the same). Right now we can run the design and see boxes being drawn around each feature points.  You can give that a try.

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    We had a lot issues setting up and run  XAPP1167 as well.   However, we did get it working by exporting the Vivado HLS code as a ISE compatible IP, than start from XAPP890 and replace the Sobel filter IP with Fast IP (all connection stays the same). Right now we can run the design and see boxes being drawn around each feature points.  You can give that a try.

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi,

    Did you start from the XAPP890 original or from the one already for ZedBoard?
    Now i'm trying to use the XAPP890 for ZedBoard, but one core is blocked and need a special license that i cannot buy. Can you help me, please?

    Thank you!