Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development UltraZed IOCC SD Card RO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 581 views
  • Users 0 members are here
Related

UltraZed IOCC SD Card RO

e14 Contributor
e14 Contributor over 9 years ago

I am working on booting the UltraZed from the SD Card of the IOCC. I have successfully built and booted linux with a custom filesystem, however I am unable to get the SD Card to mount as RW. Even using the default image that ships with the board, I am unable to mount an SD Card as RW. I have moved the SD_WP_N Jumper to both positions without any luck. 

The device tree bindings I am using are the same as provided by Avnet: Github Link

Any suggestions are greatly appreciated!

Thanks,

Ryan

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 9 years ago

    Hi Ryan,

    Have you been able to mount that same SD card when booting our Out-of-Box PetaLinux design for UltraZed IOCC?

    http://ultrazed.org/support/design/17596/131

    If not, I have run into problems with mounting some file systems in R/W mode, particularly NTFS unless the proper driver support has been built into the Linux kernel.

    Which file system are you using on the SD card?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to zedhed

    I have been able to mount both FAT and EXT4 file systems, however they only mount in Read-Only mode. Here are the steps I have attempted:

    1.   Boot OOB Image from Flash Memory with SD Card formatted as FAT/ext4)
    2.   Login Root
    3.   mount /dev/mmcblk1p1 /media
    4.   cd /media
    5.   mkdir test --> mkdir: can't create directory 'test': Read-only file system
    I've tried multiple variations of this with FAT and EXT4 file systems, both resulting in the same issue.
     
    Thanks,
    Ryan
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    For the time being, I have disabled write protection in the device tree by modifying system-top.dts.

    &sdhci1 {
      status = "okay";
      max-frequency = <50000000>;
      no-1-8-v; /* for 1.0 silicon */
      disable-wp;
    };
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer