Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Unable to detect the zedboard as device using usb interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 363 subscribers
  • Views 1800 views
  • Users 0 members are here
Related

Unable to detect the zedboard as device using usb interface

e14 Contributor
e14 Contributor over 14 years ago

Hi
I'm using the digilent linux source code and i'm able to use zedboard as host in USB interface. When i try use zedbaord as device then it is not detecting with host PC. I have removed the jumpers J2 & J3 to detect as device. But still it is failing. Could you help us to solve this issue?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Zedboard able to detect the USB thumb drive and mount operation also success.

    When i'm trying to connect the zedboard with windows host PC using the usb otg cable, windows is not showing any msg regarding found some hardware and zedboard also not showing any interrupt that it is detected by someone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Here is some additional information from the Xilinx wiki:

    http://wiki.xilinx.com/zynq-linux-driver-usb

    From the Zedboard Users Guide:

    http://www.zedboard.org/sites/default/files/documentations/ZedBoard_HW_UG_v1_6.pdf

    On page 34 is the jumper descriptions, which confirms that leaving J2 and J3 open is the correct jumper configuration.

    Are you able to confirm that the USB port that you are using on your host machine works by plugging in a different peripheral that you know works?  Such as a USB mouse or keyboard?

    Also, do you have administrative rights on your machine?  If you are on a domain, it is possible your Group Policy for your login will prevent hardware from being added to the machine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Here is some additional information from the Xilinx wiki:

    http://wiki.xilinx.com/zynq-linux-driver-usb

    From the Zedboard Users Guide:

    http://www.zedboard.org/sites/default/files/documentations/ZedBoard_HW_UG_v1_6.pdf

    On page 34 is the jumper descriptions, which confirms that leaving J2 and J3 open is the correct jumper configuration.

    Are you able to confirm that the USB port that you are using on your host machine works by plugging in a different peripheral that you know works?  Such as a USB mouse or keyboard?

    Also, do you have administrative rights on your machine?  If you are on a domain, it is possible your Group Policy for your login will prevent hardware from being added to the machine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi
    As I have mentioned earlier we kept open the J2 & J3 jumper settings.

    All other devices are detecting in the Host PC.

    We have tried the same thing with another board (not zedboard and has android), But the behavoiur is same.

    Could you help me what are the configuration parameters for driver level need to be taken care for this issue?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    So you are saying that other USB peripherals work, however the Zedboard nor a separate board running Android enumerate?  Do you have another machine that you can see if enumeration occurs on?

    The other thought I had was, is the Linux kernel you are using have the USB OTG Slave kernel module loaded.  I will take a look to see if it compiles in by default once I can RDP into my hope server.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I have customer with similar issue...

    I have a question about using the ZED board as a USB device which we would like to do. We are able to run the OTG USB demo where we mount a flash drive in Linux. In this demo the ZED is the Host. We tried setting the jumpers J2 and J3 so that the ZED board is a USB device. We plugged the USB cable into a host PC, but the ZED did not enumerate on the PC. Nothing in the device manager.