Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Unable to apply 32MB Ramdisk patch to U-boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 363 subscribers
  • Views 1815 views
  • Users 0 members are here
Related

Unable to apply 32MB Ramdisk patch to U-boot

e14 Contributor
e14 Contributor over 13 years ago

Hello all,
  I've been going through the Implementing Linux on the Zynq-7000 SoC speedway course but ran into a road block.  I completed all the labs up to lab1_2 #11 where you copy over the given patch file and apply it with the following command.

git apply 0001-Xilinx-ARM-Experimental-32MB-Ramdisk-on-ZedBoard.patch

I get the following error.

[blw184@localhost u-boot-xlnx]$ git apply 0001-Xilinx-ARM-Experimental-32MB-Ramdisk-on-ZedBoard.patch
error: patch failed: include/configs/zynq_zed.h:38
error: include/configs/zynq_zed.h: patch does not apply

Am I doing something wrong?

Thank you,
Brandon

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    If you type "git branch" into the terminal what comes up?  Xilinx have changed the way the zynq config files work so you may need to checkout an older branch.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the reply m.russell!

    [blw184@localhost u-boot-xlnx]$ git branch
      master
    * xilinx-14.2-build1-trd

    I think that's the correct build?

    I also ran into an similar problem with patching the linux-xlnx.
     
    [blw184@localhost ~]$ cd linux-xlnx/
    [blw184@localhost linux-xlnx]$ git apply 0001-Xilinx-ARM-Kernel-32MB-RAM-disk-on-ZedBoard.patch
    warning: arch/arm/configs/xilinx_zynq_defconfig has type 100755, expected 100644

    Thanks,
    Brandon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    With regards to the similar problem with patching the linux-xlnx.  The tutorial did say "Ignore any warnings about file permissions or types."  So I'm assuming that error is OK.

    Brandon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Yep, that's the right one.  I just ran through that part of the speedway and it worked OK for me.  Try to clone the repository again, check out xilinx-14.2-build1-trd, and apply the patch on a clean version.

    The warning with the Linux patch isn't a problem.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Which steps did you exactly perform/what do you mean with "clean version"?
    I have the same problem with the patch and I get the same message after "git branch" but when I try the "make" command I get this error message:
    ------------------------------------------------
    [training@localhost u-boot-xlnx]$ make
    make: arm-linux-gcc: Command not found
    /bin/sh: arm-linux-gcc: command not found
    dirname: missing operand
    Try `dirname --help' for more information.
    Generating include/autoconf.mk
    /bin/sh: line 3: arm-linux-gcc: command not found
    Generating include/autoconf.mk.dep
    /bin/sh: line 3: arm-linux-gcc: command not found
    make: arm-linux-gcc: Command not found
    /bin/sh: arm-linux-gcc: command not found
    dirname: missing operand
    Try `dirname --help' for more information.
    /bin/sh: arm-linux-gcc: command not found
    /bin/sh: arm-linux-ld: command not found
    arm-linux-gcc -DDO_DEPS_ONLY
    tt-g  -Os   -fno-common -ffixed-r8 -msoft-float  -fno-strict-aliasing -mno-unaligned-access -D__KERNEL__ -I/home/theil/u-boot-xlnx/include -fno-builtin -ffreestanding -nostdinc -isystem  -pipe  -DCONFIG_ARM -D__ARM__    -march=armv5  -I/home/training/u-boot-xlnx/board/xilinx/common -Wall -Wstrict-prototypes      
    tt-o lib/asm-offsets.s lib/asm-offsets.c -c -S
    make: arm-linux-gcc: Command not found
    make: *** [lib/asm-offsets.s] Error 127
    ------------------------------------------------
    Did you have the same problem or is this something different?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    It looks like you've set the CROSS_COMPILE variable to arm-linux-, it should be arm-xilinx-linux-gnueabi-.  The command to change this is:

    export CROSS_COMPILE=arm-xilinx-linux-gnueabi-

    By a clean version I mean one which has had "make distclean" run on it, this removes any config or build files which may cause problems.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    My CROSS_COMPILE variable is set to arm-xilinx-linux-gnuabi, this is my .bash_profile without any changes:
    ----------------------------------------------------
    # .bash_profile

    # Get the aliases and functions
    if [ -f ~/.bashrc ]; then
            . ~/.bashrc
    fi

    # User specific environment and startup programs

    PATH=$PATH:$HOME/bin

    export PATH
    export CROSS COMPILE=arm-xilinx-linux-gnueabi-

    # New environment setting added by Sourcery CodeBench Lite for Xilinx GNU/Linux on Wed Jan 30 23:47:50 PST 2013 1.
    # The unmodified version of this file is saved in /home/training/.bash_profile1042213503.
    # Do NOT modify these lines; they are used to uninstall.
    PATH="/home/training/CodeSourcery/Sourcery_CodeBench_Lite_for_Xilinx_GNU_Linux/bin:${PATH}"
    export PATH
    # End comments by InstallAnywhere on Wed Jan 30 23:47:50 PST 2013 1.
    ".bash_profile" 20L, 653C                                     1,1           All
    ----------------------------------------------------
    I have still the problem with the patch described in the first commend, even when I clone the u-boot-xlnx directory again and make a distclean, could it be that this is the source of all my problems?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The error with the patch would not cause the make errors, it would just build the un-patched u-boot file.  If you type "echo $CROSS_COMPILE" and "echo $PATH" into the bash terminal what comes up?

    If all else fails, the patch file is human readable.  You can open it using a text editor and apply the changes yourself, it's only a few lines.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    It works now, I just installed linux again and repeated the complete process but it's really confusing why it have not worked for the first time...

    Thank you for your help
    Tobias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I did exactly what you suggested and this time it worked.
    Thank you so much.
    Brandon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>