Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Unable to apply 32MB Ramdisk patch to U-boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 363 subscribers
  • Views 1817 views
  • Users 0 members are here
Related

Unable to apply 32MB Ramdisk patch to U-boot

e14 Contributor
e14 Contributor over 13 years ago

Hello all,
  I've been going through the Implementing Linux on the Zynq-7000 SoC speedway course but ran into a road block.  I completed all the labs up to lab1_2 #11 where you copy over the given patch file and apply it with the following command.

git apply 0001-Xilinx-ARM-Experimental-32MB-Ramdisk-on-ZedBoard.patch

I get the following error.

[blw184@localhost u-boot-xlnx]$ git apply 0001-Xilinx-ARM-Experimental-32MB-Ramdisk-on-ZedBoard.patch
error: patch failed: include/configs/zynq_zed.h:38
error: include/configs/zynq_zed.h: patch does not apply

Am I doing something wrong?

Thank you,
Brandon

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    It looks like you've set the CROSS_COMPILE variable to arm-linux-, it should be arm-xilinx-linux-gnueabi-.  The command to change this is:

    export CROSS_COMPILE=arm-xilinx-linux-gnueabi-

    By a clean version I mean one which has had "make distclean" run on it, this removes any config or build files which may cause problems.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    It looks like you've set the CROSS_COMPILE variable to arm-linux-, it should be arm-xilinx-linux-gnueabi-.  The command to change this is:

    export CROSS_COMPILE=arm-xilinx-linux-gnueabi-

    By a clean version I mean one which has had "make distclean" run on it, this removes any config or build files which may cause problems.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    My CROSS_COMPILE variable is set to arm-xilinx-linux-gnuabi, this is my .bash_profile without any changes:
    ----------------------------------------------------
    # .bash_profile

    # Get the aliases and functions
    if [ -f ~/.bashrc ]; then
            . ~/.bashrc
    fi

    # User specific environment and startup programs

    PATH=$PATH:$HOME/bin

    export PATH
    export CROSS COMPILE=arm-xilinx-linux-gnueabi-

    # New environment setting added by Sourcery CodeBench Lite for Xilinx GNU/Linux on Wed Jan 30 23:47:50 PST 2013 1.
    # The unmodified version of this file is saved in /home/training/.bash_profile1042213503.
    # Do NOT modify these lines; they are used to uninstall.
    PATH="/home/training/CodeSourcery/Sourcery_CodeBench_Lite_for_Xilinx_GNU_Linux/bin:${PATH}"
    export PATH
    # End comments by InstallAnywhere on Wed Jan 30 23:47:50 PST 2013 1.
    ".bash_profile" 20L, 653C                                     1,1           All
    ----------------------------------------------------
    I have still the problem with the patch described in the first commend, even when I clone the u-boot-xlnx directory again and make a distclean, could it be that this is the source of all my problems?