Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development petalinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1373 views
  • Users 0 members are here
Related

petalinux

yangtuzi
yangtuzi over 9 years ago

I want to make image by petalinux.

I do step fallow ug1144

1.source /home/petalinux/settings.sh

2.echo $PETALINUX

3.petalinux-create --type project --template zynq --name test

4.petalinux-config --get-hw-description=/home/design_1_wrapper_hw_platform_0

5.petalinux-build

then ERROR appears:

ERROR:OE-core's config sanity checker detected a potential misconfiguration.Either fix the cause of this error or at your own risk disable the checker(see sanity.conf).Following is the list of potential problems/advisories:

Do not use Bitbake as root.

How can I solve this error?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 9 years ago

    Hi yangtuzi,

    Are you running petalinux-build as root?

    PetaLinux requires installation by a non-root user and Xilinx recommends installing 2017.1 into a the users home folder.

    To be consistent with older approaches we have taken with PetaLinux, we have an updated "VirtualBox and Linux VM Installation Guide v2017.1" on this page which can help you setup the PetaLinux tools on your machine:

    http://microzed.org/support/design/18891/146

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • yangtuzi
    0 yangtuzi over 9 years ago in reply to zedhed

    I install petalinux by non-root user and installing petalinux 2017.2 into a /home/xxxx0(we OS is redhat6.7,and many user folder in /home)

    when:

    petalinux-config --get-hw-description=/home/xxxx0/xxx_platform_0/

    then error appears:

    [INFO] sourceing bitbake

    ERROR:Failed to source bitbake

    ERROR:Failed to config project

    ERROR:Get hw description Failed!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 8 years ago

    Hi yangtuzi,

    Check out this thread on the Xilinx forums where others were experiencing a similar problem that was related to an incorrect version of Python being installed:

    https://forums.xilinx.com/t5/Embedded-Linux/Petalinux-2017-2-Failed-to-source-bitbake/td-p/796848/page/2

    Is it possible this is also the cause of your issue with bitbake?

    Best Regards,

    -Kevin